cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo l152RE virtual com port not work

bfran.1
Associate II

I have my Nucleo l152RE board i want send and receive small data using vpc , then i use cdc configuration then my program :

 MX_GPIO_Init();

 MX_USART2_UART_Init();

 MX_USB_DEVICE_Init();

 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */

 /* USER CODE BEGIN WHILE */

 while (1)

 {

  /* USER CODE END WHILE */

  /* USER CODE BEGIN 3 */

  HAL_Delay(1000);

  uint8_t buffer[] = "Hello, World!\r\n";

  CDC_Transmit_FS(buffer, sizeof(buffer));

  HAL_Delay(1000);

   

   

   

 }

Im using just a cable usb connected to CN1 i have Sb63 e sb62 OFF , when i run my code in my device on Windows 10 I see just Stilink virtual port COM7 , and on tera term i don't see nothing , I Have tried to interface another usb cable interfaced to pa11 , pa12 gnd and 5 V but also in this case I dont see nothig .

Can help me.

Thanks

Francesco

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
NorfLoud
Associate III

Hello.

Have you got this error "../Src/main.c:126:2: warning: implicit declaration of function 'CDC_Transmit_FS' [-Wimplicit-function-declaration]"?

If yes, then try "#include "usbd_cdc_if.h"" in section "/* USER CODE BEGIN Includes */"