Nucleo l152RE virtual com port not work
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-07-21 4:59 AM
I have my Nucleo l152RE board i want send and receive small data using vpc , then i use cdc configuration then my program :
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_USB_DEVICE_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_Delay(1000);
uint8_t buffer[] = "Hello, World!\r\n";
CDC_Transmit_FS(buffer, sizeof(buffer));
HAL_Delay(1000);
}
Im using just a cable usb connected to CN1 i have Sb63 e sb62 OFF , when i run my code in my device on Windows 10 I see just Stilink virtual port COM7 , and on tera term i don't see nothing , I Have tried to interface another usb cable interfaced to pa11 , pa12 gnd and 5 V but also in this case I dont see nothig .
Can help me.
Thanks
Francesco
- Labels:
-
STM32F1 Series
-
USB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-08-05 11:22 AM
Hello.
Have you got this error "../Src/main.c:126:2: warning: implicit declaration of function 'CDC_Transmit_FS' [-Wimplicit-function-declaration]"?
If yes, then try "#include "usbd_cdc_if.h"" in section "/* USER CODE BEGIN Includes */"