Non blocking or Event base programming for MCU in C is possible?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-02-07 4:59 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-02-07 6:00 AM
Use an RTOS and semaphore, signal, etc.
instead of active waiting the RTOS will switch tasks until the resouce is available or the delay expired.
And don't use active waiting like HAL_Delay()!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-02-07 6:07 AM
Or use an interrupt to perform the task while letting the main loop do less important tasks. Implementation will depend on your exact needs. Small frequent tasks will be best served by an interrupt.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-02-07 7:35 AM
You can also do it without RTOS or interrupt; eg,
// flag to be set by the long-running process when it completes
bool long_running_process_completed = false;
initiate_long_running_process();
:
:
// do other stuff while process runs
:
:
if( long_running_process_completed )
{
// handle completion
}
else
{
// do some more other stuff while process still runs
}
State Machines (aka Finite State Machines, FSM) give another approach ...
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-02-07 8:21 AM
One more vote for state machines (coming from FPGAs and almost zero knowledge about OS...) plus interrupts.
Put one in main(), and every function called in main, use flags.
For high priority stuff check according flags in main outside of state machine.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-02-07 9:39 AM
Yes.
This is "Cooperative multitasking".
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-02-07 7:18 PM
To answer the question, C can generate assembly code, so yes. Now without RTOS, if the goal is not keeping the core self warming and plan low power mode in the next quest, use interrupts. More specificallu use a state machine that gets kicked by chosen interrupt signals. For example, EXTI and SPI and DMA interrupt events going to the FSM to perform SPI slave. If need delays, feed the FSM with timer compare interrupts. All the sources should be having same IRQ priority. This way, smarter peripherals can be built under a bare metal or an OS.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-02-08 1:46 AM
(NO RTOS)
For nonblocking delays i always use HAL_GetTick()
its similar to the millis() funtion in arduino
And do something like this for a periodic 500ms task (not as precise as interruptions and sccesptible to delays in your firmware.
uint32_t lastGetTick;
.....
//check if 500ms passed since last time this if() was triggered
if((HAL_GetTick()-lastGetTick)>=500){
//do your thing
//reset the tick
lastGetTick=HAL_GetTick()
}
.....
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-02-08 4:50 AM - last edited on 2023-12-18 11:37 AM by Peter BENSCH
You have to be careful with this. Have a look to: https://community.st.com/s/question/0D50X00009XkgXi/years-on-continue-to-see-the-same-bad-timeout-code
It is better to do a subtraction for each loop
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-02-08 9:21 AM
thanks @Nikita91 i changed my example