cancel
Showing results for 
Search instead for 
Did you mean: 

Maximum sampling on USB audio class 1.0

Stabilo
Associate III

Hello,

Is it possible to use USB full speed (12 Mbit/s) combined with audio class 1.0 to transfer 16bit audio data sampled at 384ksps ?

According to my calculation, I need to transfer 768 bytes/ms over USB:

384000 * 16 = 6144000 bits/s

= 6144 bits/ms

= 768 bytes/ms

So in theory, it fits in the 1024 bytes/ms restriction of the USB full speed.

But the usb audio class 1.0 stands that the maximum sample rate is 78 kHz...

Is it possible to achieve transferring 16bits data at 384ksps ?

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions

But for example drivers in PC dont support this on UAC1

View solution in original post

4 REPLIES 4
MM..1
Chief III

Yes one channel mono as you see or stereo on 192k max but ...

Stabilo
Associate III

But ? :)

Is it tricky to implement ?

But for example drivers in PC dont support this on UAC1

Thank you for the information !