2022-01-12 10:08 PM
MCU is STM32F207VIT6 (client)
server is windows application.
LWIP library is used.
Is there any ping command?
2022-01-12 10:33 PM
Ping:
Yes, there is, and it's "processed" in icmp.c as ICMP_ECHO .
So you must have LWIP_ICMP defined to enable ping, in opt.h .
2022-01-12 11:02 PM
already set to 1. Will you please elaborate more.
2022-01-15 2:31 PM
https://www.nongnu.org/lwip/2_1_x/tcp_8h.html#a780cfac08b02c66948ab94ea974202e8
Parameters
p The received data (or NULL when the connection has been closed!)
Either that or this:
https://www.nongnu.org/lwip/2_1_x/tcp_8h.html#a1b4f9e3551e575c0ef06d6daa7f06e55