2024-08-06 11:09 AM
This is another issue found in my endeavors to learn Zephyr. When building I get the following error:
warning: orphan section `.stm32_sdram2' from `zephyr/drivers/display/libdrivers__display.a(display_stm32_ltdc.c.obj)' being placed in section `.stm32_sdram2'
section `.stm32_sdram2' will not fit in region `IDT_LIST'
section .stm32_sdram2 VMA wraps around address space
region `IDT_LIST' overflowed by 228513 bytes
collect2.exe: error: ld returned 1 exit status
Here's my DTS setup:
&fmc {
pinctrl-0 = <&fmc_nbl0_pe0 &fmc_nbl1_pe1
&fmc_sdclk_pg8 &fmc_sdnwe_ph5 &fmc_sdcke1_ph7
&fmc_sdne1_ph6 &fmc_sdnras_pf11 &fmc_sdncas_pg15
&fmc_a0_pf0 &fmc_a1_pf1 &fmc_a2_pf2 &fmc_a3_pf3 &fmc_a4_pf4
&fmc_a5_pf5 &fmc_a6_pf12 &fmc_a7_pf13 &fmc_a8_pf14
&fmc_a9_pf15 &fmc_a10_pg0 &fmc_a11_pg1
&fmc_a12_pg2 &fmc_d0_pd14 &fmc_d1_pd15
&fmc_d2_pd0 &fmc_d3_pd1 &fmc_d4_pe7 &fmc_d5_pe8 &fmc_d6_pe9
&fmc_d7_pe10 &fmc_d8_pe11 &fmc_d9_pe12 &fmc_d10_pe13
&fmc_d11_pe14 &fmc_d12_pe15 &fmc_d13_pd8 &fmc_d14_pd9
&fmc_d15_pd10>;
pinctrl-names = "default";
status = "okay";
sdram {
status = "okay";
power-up-delay = <100>;
num-auto-refresh = <8>;
mode-register = <0x220>;
refresh-rate = <0x2F9>;
bank@1 {
reg = <1>;
st,sdram-control = <STM32_FMC_SDRAM_NC_9
STM32_FMC_SDRAM_NR_13
STM32_FMC_SDRAM_MWID_16
STM32_FMC_SDRAM_NB_4
STM32_FMC_SDRAM_CAS_2
STM32_FMC_SDRAM_SDCLK_PERIOD_2
STM32_FMC_SDRAM_RBURST_ENABLE
STM32_FMC_SDRAM_RPIPE_2>;
st,sdram-timing = <2 7 5 7 3 2 2>;
};
};
};
<dc {
status = "okay";
pinctrl-0 = <<dc_r0_pi15 <dc_r1_pj0 <dc_r2_pj1 <dc_r3_pj2
<dc_r4_pj3 <dc_r5_pj4 <dc_r6_pj5 <dc_r7_pj6
<dc_g0_pj7 <dc_g1_pj8 <dc_g2_pj9 <dc_g3_pj10
<dc_g4_pj11 <dc_g5_pk0 <dc_g6_pk1 <dc_g7_pk2
<dc_b0_pj12 <dc_b1_pj13 <dc_b2_pj14 <dc_b3_pj15
<dc_b4_pk3 <dc_b5_pk4 <dc_b6_pk5 <dc_b7_pk6
<dc_de_pk7 <dc_clk_pi14 <dc_hsync_pi12 <dc_vsync_pi13>;
pinctrl-names = "default";
disp-on-gpios = <&gpioi 10 GPIO_ACTIVE_HIGH>;
bl-ctrl-gpios = <&gpioc 6 GPIO_ACTIVE_HIGH>;
/*
lcd-intr-gpios = <&gpiog 2 GPIO_ACTIVE_HIGH>;
lcd-rst-gpios = <&gpiob 12 GPIO_ACTIVE_HIGH>;
*/
/*eternal SDRAM in which frame buffer will be stored.If not defined, internal RAM will be used. */
/*refer st,stm32-ltdc.yml*/
ext-sdram = <&sdram2>;
/*PANEL_PIXEL_FORMAT_RGB_888*/
/*pixel-format = <1>;*/
width = <480>;
height = <272>;
display-timings {
compatible = "zephyr,panel-timing";
de-active = <0>;
pixelclk-active = <0>;
hsync-active = <0>;
vsync-active = <0>;
hsync-len = <1>;
vsync-len = <1>;
hback-porch = <88>;
vback-porch = <32>;
hfront-porch = <40>;
vfront-porch = <13>;
};
pixel-format = <PANEL_PIXEL_FORMAT_RGB_565>;
def-back-color-red = <0xFF>;
def-back-color-green = <0xFF>;
def-back-color-blue = <0xFF>;
};
sdram2: sdram@d0000000 {
compatible = "zephyr,memory-region", "mmio-sram";
device_type = "memory";
reg = <0xd0000000 DT_SIZE_M(32)>; /* 256Mbit */
zephyr,memory-region = "SDRAM2";
zephyr,memory-attr = <( DT_MEM_ARM(ATTR_MPU_RAM_NOCACHE) )>;
};
&sdram2 {
status = "okay";
};
Any advice/pointer is appreciated. Thanks!
2024-08-07 06:53 AM
Hello Xavier,
The error you're getting suggests that the section .stm32_sdram2 is not fitting in the region IDT_LIST
the address 0xd0000000 and the size DT_SIZE_M(32) shouldn't overlap with other mem regions.
Check if the linker script includes sdram2 region and it's properly sized.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-12 11:45 AM
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy
2025-01-09 08:49 AM - edited 2025-01-09 09:21 AM
Hi @Billy OWEN,
Currently i am also facing the exact same issue, can you please share the solution here.
Regards,
Ganesh