Skip to main content
Singh.Harjit
Senior
November 16, 2019
Question

Is .fpu incorrect in startup_stm32f411xe.s?

  • November 16, 2019
  • 10 replies
  • 3163 views

In startup_stm32f411xe.s, the FPU seems to be incorrectly declared. It is:

.fpu softvfp

Shouldn't it be:

.fpu fpv4-sp-d16

I checked other files in the same family and they also have the softvfp declaration.

This topic has been closed for replies.

10 replies

Tesla DeLorean
Guru
November 17, 2019

Is it throwing a warning at link time?

Do you actually have any FPU instructions in the start-up assembler?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Singh.Harjit
Senior
November 17, 2019

I'm not getting any warnings.

I don't have any FPU instructions in the startup code.

I do enable and use the FPU in startup code.

I was concerned about declaring incorrect / inconsistent FPU information with the rest of the code base.

Tesla DeLorean
Guru
November 17, 2019

I don't think this is consequential.

If you use FPU instructions in the file you'll need to pick a hardware options that covers the instructions in question, so things like push/pop of the float/double registers don't throw errors, for example.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate II
August 10, 2024

I checked everything today and worked as expected. Thanks.

Just moved from a custom board that used STMG0 to a STM32H723. I am so ecstatic to finally be able to figure out TCM, Cache Write back, and just trying to unlock every bit of performance. Kind of bit more than i can chew with a huge project but it feels like i have injected crack. Its fun.