IRDA Communication Problem - Unreasonable Recieved Data
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-23 7:16 AM
Hi,
I'm trying to use simple IRDA IT communication.
I am using Interrupt to receive data. I set for 7 bytes to receive data and when 6th array character is taken, I transmit data. But with second cycle, the received data is crashed by somethings. If receive data is used alone without transmit, then there is no problem, However, while either receive and transmit functions are used, the received data became unreasonable. I use HAL functions How can I fix it?The MCU is STM32L031G6Ux
the crashed Data is 'L;S&~�?' instead of '1234567'
main.c ----- setting Recieve Data
UART_HandleTypeDef hlpuart1;
IRDA_HandleTypeDef hirda2;
TIM_HandleTypeDef htim22;
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_IRDA_Init(void);
static void MX_LPUART1_UART_Init(void);
static void MX_TIM22_Init(void);
uint32_t count=0;
uint8_t RecievedData[7];
uint8_t FinalData[7];
uint8_t TransmitedData[] = 'Hello world!';
HAL_IRDA_StateTypeDef stat;
HAL_StatusTypeDef status;int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART2_IRDA_Init(); MX_LPUART1_UART_Init(); MX_TIM22_Init();HAL_TIM_Base_Init(&htim22);
HAL_TIM_Base_Start(&htim22);HAL_IRDA_Receive_IT(&hirda2, RecievedData, sizeof(RecievedData));
while (1)
{if (button == true)
{
HAL_IRDA_Transmit(&hirda2, TransmitedData, strlen(TransmitedData)-1, 100);
}
}
}
... Other initialization
stm3210xx_it.c ------- Interrupt wait for data ------
Recieve function is set for 7 bytes
void USART2_IRQHandler(void)
{ /* USER CODE BEGIN USART2_IRQn 0 */ count = __HAL_TIM_GET_COUNTER(&htim22);// If time between two recieved data is bigger than 100 ms
if (count > 100 )// then reset RecievedData Array
{// Because, Sometimes data is '
1234
' instead of '1234567
'/
/ And assume that second data is '
1234567
'memset(RecievedData, 0, 7);
// In this case with second data, function give me '
1234
123
'IRDA_EndRxTransfer(&hirda2);
// And it continue in this synchronous (next data '
4567
123
')
IRDA_EndTxTransfer(&hirda2);// This Block prevents this situation
} /* USER CODE END USART2_IRQn 0 */ HAL_IRDA_IRQHandler(&hirda2); /* USER CODE BEGIN USART2_IRQn 1 */ stat = HAL_IRDA_GetState(&hirda2); if (stat== HAL_IRDA_STATE_READY && RecievedData[6] != 0) { for (int i=0; i<7; i++)// if 7 bytes come, The recieve array to final array
{ FinalData[i]= RecievedData[i]; } memset(RecievedData, 0, 7);// Reset array
} if (stat== HAL_IRDA_STATE_RESET) { memset(RecievedData, 0, 7); } __HAL_TIM_SET_COUNTER(&htim22, 0);// Reset Counter
HAL_IRDA_Receive_IT(&hirda2, RecievedData, 7);// set Interruprt for next interrupt
/* USER CODE END USART2_IRQn 1 */}#hal-usart #hal #rx #irda #tx #hal-uartSolved! Go to Solution.
- Labels:
-
STM32Cube MCU Packages
-
UART-USART
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-25 11:12 PM
How do you init the IRDA peripheral ? I had similar issues with a bad init. Use a 115200 baudrate, 8 bit, prescaler to 1, no parity on both sides of course.
Here is my init :
/* USART1 init function */
static void MX_USART1_IRDA_Init(void){hirda1.Instance = USART1;
hirda1.Init.BaudRate = 115200; hirda1.Init.WordLength = IRDA_WORDLENGTH_8B; hirda1.Init.Parity = IRDA_PARITY_NONE; hirda1.Init.Prescaler = 1; hirda1.Init.PowerMode = IRDA_POWERMODE_NORMAL; hirda1.Init.Mode = IRDA_MODE_TX_RX; if (HAL_IRDA_Init(&hirda1) != HAL_OK) { Error_Handler(); }}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-23 8:06 AM
Don't really see many IRDA questions these days.
You might need to more actively manage the state of your driver as the medium is half-duplex.
You could perhaps dig through some of the EVAL board support code, with from HAL, or earlier SPL, for IRDA examples.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-25 10:24 PM
Actually, I set the prameters and functions via CubeMX and I tried simple example but it had same problem. Then, I have tried to fix problem but there is no way for solution which i could find. I really need to help. I added my source code to attachment.
________________ Attachments : IRDA.rar : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hxs2&d=%2Fa%2F0X0000000b1Z%2FdHK7zG0KC8xG10.e_YfgUGt5A3PBy1.Oxuf14F7tqAA&asPdf=false- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-25 11:12 PM
How do you init the IRDA peripheral ? I had similar issues with a bad init. Use a 115200 baudrate, 8 bit, prescaler to 1, no parity on both sides of course.
Here is my init :
/* USART1 init function */
static void MX_USART1_IRDA_Init(void){hirda1.Instance = USART1;
hirda1.Init.BaudRate = 115200; hirda1.Init.WordLength = IRDA_WORDLENGTH_8B; hirda1.Init.Parity = IRDA_PARITY_NONE; hirda1.Init.Prescaler = 1; hirda1.Init.PowerMode = IRDA_POWERMODE_NORMAL; hirda1.Init.Mode = IRDA_MODE_TX_RX; if (HAL_IRDA_Init(&hirda1) != HAL_OK) { Error_Handler(); }}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-26 3:38 AM
it can not work 115200 baudrate, it is 9600 in two side. After the prescaler value it correctly work (still 9600). Thank you
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-26 12:47 PM
Thanks for the tip. The prescaler was set to 10 by the CubeMX configuration, baud rate 9600.The IrDA received lots of misread values. Once the prescaler was changed to 1, there were no misread values, all were correctly read.
I am not clear on what is the purpose of the prescaler. Is it a clock divider to achieve the desired baud rate? Or is it a parameter for filtering out glitches?