2021-03-30 10:06 PM
hello all
currently i am working on Free RTOS (STM32L152RETX microcontroller ) . in stmcubemx no any one feature to implement the any protocal like TCP/ip etc
is there any possiblities to implement this protocal by using STM32L152RETx microcontroller
if yes then how
2021-03-31 1:31 AM
The L15x MCUs have no ethernet MAC, so no.
There will be no direct support by ST or ST tools.
But third-party vendors offer boards or companion chips implementing ethernet/TCP-IP, and translate it to one of the usual serial protocols.
I remember Microchip had one of those, can't remember the type name - I never used it.
That adds quite a bit to the BOM, though.
2021-04-06 4:25 AM
okk sir
2021-04-06 4:25 AM
i will try