cancel
Showing results for 
Search instead for 
Did you mean: 

I am using a STM407VET6 development board, and when I connect it via USB, it is recognized as "STM32 ST-Link" as a USB device, but not as a VCP. How can I solve this problem?

tacchi
Associate II
 
18 REPLIES 18

Perhaps connect to the other USB port?

If this is the STM32F407-DISCO board, the TOP/NORTH connector goes to an STM32F1

The BOTTOM/SOUTH Micro-AB connects to the STM32F4, and whatever software you have running on that.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
KnarfB
Principal III

Try re-installing all drivers.

hth

KnarfB

tacchi
Associate II

TOP/NORTH connector to a desktop PC.

The driver has already been reinstalled.

When other boards (F407G-DISC, NUCLEO-F446RE) are connected, they are recognized as VCP.

The driver has already been reinstalled.

When other boards (F407G-DISC, NUCLEO-F446RE) are connected, they are recognized as VCP.

I connect TOP/NORTH connector to a desktop PC.

also did other connector.

The driver has already been reinstalled.

When other boards (F407G-DISC, NUCLEO-F446RE) are connected, they are recognized as VCP.

> I am using a STM407VET6 development board

What board? Post photo.

JW​

0693W00000QMp2GQAT.jpgI'm using​ this board.

KnarfB
Principal III

This board has a ST-LINK/V2-A which does not include VCP. See

STM32F4DISCOVERY Data brief and

TN1235 Overview of the ST-LINK versions.

hth

KnarfB

KnarfB
Principal III

Can add VCP by soldering 2 wires, see UM1472 Discovery kit with STM32F407VG MCU

hth

KnarfB