cancel
Showing results for 
Search instead for 
Did you mean: 

USBX-Host on NUCLEO-U575ZI

laltobelli
Associate

Is there any working example for this board (NUCLEO-U575ZI) where I can learn how to write files on a USB Hard Drive connected over the USB-Type C port using USBX and FILEX?

On CubeIDE I found an example Ux_Host_MSC regarding STM32U575I-EV but cannot make it work on the Nucleo board.

Regards

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Mohamed Aymen HZAMI
ST Employee

Hello @laltobelli​ and welcome to the community,

The example you mentioned of the STM32U575I-EV board provide two threads:

  • thread one: file system on µSD using FileX stack
  • thread two: file system on OSPI NOR Flash using FileX/LevelX stacks

For your case you can refer to both cases on how to implement the FileX stack to your specific case.

Mohamed Aymen

laltobelli
Associate

Hi Mohamed,

thank you for your reply.

What I'm really looking for is:

  • can I use Ux_Host_MSC over the USB-Type C on NUCLEO-U575ZI board?
  • if yes, is there any example? Where?

Regards

Luca