2019-10-21 1:58 AM
Hello,
I'm trying to send some data via UART and DMA on a STM32F072, but with the low level functions. This works perfectly when using the HAL-function HAL_UART_Transmit_DMA(), but I'm missing some information for the low level functions. I configured everything with CubeMX and have this example "code" running:
// Disable DMA to load new length to be tranmitted
LL_DMA_DisableChannel(DMA1, LL_DMA_CHANNEL_4);
// set length to be tranmitted
volatile uint8_t uart60_tx_buffer[10] = {1, 2, 3, 4, 5, 6, 7, 8, 9, 10};
LL_DMA_SetDataLength(DMA1, LL_DMA_CHANNEL_4, sizeof(uart60_tx_buffer) );
// configure address to be transmitted by DMA
LL_DMA_ConfigAddresses(DMA1, LL_DMA_CHANNEL_4, (uint32_t)uart60_tx_buffer, (uint32_t)LL_USART_DMA_GetRegAddr(USART2, LL_USART_DMA_REG_DATA_TRANSMIT), LL_DMA_GetDataTransferDirection(DMA1, LL_DMA_CHANNEL_4));
// Enable DMA again
LL_DMA_EnableChannel(DMA1, LL_DMA_CHANNEL_4);
// how to start sending with DMA?!
// this works, but is not with DMA support
LL_USART_TransmitData8( USART2, 'A');
I'm just missing the command of function, with which the transmission of the data in the array uart60_tx_buffer[10] is acctually been send. Is this even possible with the low level functions?
Thanks in advance
Solved! Go to Solution.
2019-10-21 3:50 AM
2019-10-21 2:54 AM
Steps to be considered (in order):
Best regards,
Tilen
2019-10-21 3:48 AM
Hello, thank you for your replay. Can you please clarify the step "Enable UART DMA TX request" in a bit more detail? This ist my basic question, what is the function call for this, I was not able to find it by my own...
2019-10-21 3:50 AM
Function name is LL_USART_EnableDMAReq_TX.
Tilen
2023-08-01 4:25 AM
Hi Tilen,
I have a problem with getting data on RX with DMA, Am i doing it correct?
LL_USART_EnableIT_RXNE(USART2);
LL_USART_IsEnabledIT_IDLE(USART2);
LL_DMA_ConfigAddresses(DMA1, LL_DMA_CHANNEL_1, (uint32_t)usart_rx_dma_buffer, (uint32_t)LL_USART_DMA_GetRegAddr(USART2, LL_USART_DMA_REG_DATA_TRANSMIT), LL_DMA_GetDataTransferDirection(DMA1, LL_DMA_CHANNEL_1));
LL_DMA_SetDataLength(DMA1, LL_DMA_CHANNEL_1, sizeof(usart_rx_dma_buffer) );
LL_USART_EnableDMAReq_RX(USART2);
LL_USART_EnableDirectionRx(USART2);
LL_USART_Enable(USART2);
LL_DMA_EnableChannel(DMA1, 1);
void DMA1_Channel1_IRQHandler(void) {
/* Check half-transfer complete interrupt */
if (LL_DMA_IsEnabledIT_HT(DMA1, LL_DMA_CHANNEL_1) && LL_DMA_IsActiveFlag_HT1(DMA1)) {
LL_DMA_ClearFlag_HT1(DMA1); /* Clear half-transfer complete flag */
usart_rx_check(); /* Check for data to process */
}
/* Check transfer-complete interrupt */
if (LL_DMA_IsEnabledIT_TC(DMA1, LL_DMA_CHANNEL_1) && LL_DMA_IsActiveFlag_TC1(DMA1)) {
LL_DMA_ClearFlag_TC1(DMA1); /* Clear transfer complete flag */
usart_rx_check(); /* Check for data to process */
}
/* Implement other events when needed */
}
/**
* \brief USART3 global interrupt handler
*/
void USART2_IRQHandler(void) {
/* Check for IDLE line interrupt */
if (LL_USART_IsEnabledIT_IDLE(USART2) && LL_USART_IsActiveFlag_IDLE(USART2)) {
LL_USART_ClearFlag_IDLE(USART2); /* Clear IDLE line flag */
usart_rx_check(); /* Check for data to process */
}
/* Implement other events when needed */
}
2023-08-07 11:57 AM
The second line of your code doesn't enable the IDLE interrupt.
2023-08-21 6:59 AM
Thank you for your replay, i am not using the LL anymore but het HAL instead