2021-07-07 12:47 AM
Hello everybody,
I have set an STM32469I Discovery as USB HOST MSC which has a SD card slot available. My idea is transfer all files contained in any USB flash drive connected to the USB port into the SD card ( supposing there is enough space capacity) and include some process to measure transfer speed.
Can anyone point me in the right direction regarding the process I should follow and the libraries I should use to pull this task off ?
Thank you guys for your help. I am starting in this STM32 world and very excited about it
2021-07-07 8:33 PM
I am not sure if I should do it file by file or copying by blocks( This concept I am not sure how to convert these blocks of data back into files). Conversion from blocks to files is automatic or should I do additional process to achieve it ? or is not doable in this way ? Help please
2021-07-07 9:01 PM
Depends on how involved you want to get with file system structures.
Most straight forward would be to use FatFs, enumerate through files, do a block/cluster sized copies. Duplicating timestamps and attributes
Perhaps skipping files that already exist.
Presume you want to replicate directory trees and content.
2021-07-07 11:58 PM
Thank you Mr, DeLorean,
My goal is to replicate directory trees and content at the higher speed possible. Considering I am just learning, have to start with the easiest way (FatFS is easier for me to understand) and fine tune step by step. All clear but doing "a block/cluster sized copies...", well guess I have to make my own research on this.