2024-01-04 09:45 AM - edited 2024-01-09 02:45 AM
Hi,
I am trying to understand Trustzone concepts by building my own project. I’m using STM32U5-EVK and I went through the example project(GTZC_MPCWM_IllegalAccess_TrustZone project)to understand the basics. However, in this project, I noticed that they have not enabled the SAU in .ioc file, but still the SAU_CTRL_ENABLE macro has been set to 1. Also, on debugging I saw that all the SAU regions are initialised as well.
But when I leave the SAU disabled in .ioc, the SAU ENABLE bit is 0 and SAU regions are not initialised. Could someone please explain this? Or am I missing something? Is there any other place where we can configure SAU?
Solved! Go to Solution.
2024-01-10 04:21 AM
Hello @neetha_jyo98 ,
In STM32U5, IDAU is used for default configuration of secure applications.
When SAU disabled, the default memory mapping is inherited from hardware IDAU mapping.
This IDAU memory mapping is detailed in Figure 3 of STM32U5 reference manual RM0456.
In this case, no needed for any SW development (SAU configuration) from User side to get a security mapping.
You could choose to have your own security memory mapping, then you should activate SAU in partition_stm32u5.h file (default SAU regions split are proposed in partition_stm32u5.h file, to be customized).
2024-01-10 04:21 AM
Hello @neetha_jyo98 ,
In STM32U5, IDAU is used for default configuration of secure applications.
When SAU disabled, the default memory mapping is inherited from hardware IDAU mapping.
This IDAU memory mapping is detailed in Figure 3 of STM32U5 reference manual RM0456.
In this case, no needed for any SW development (SAU configuration) from User side to get a security mapping.
You could choose to have your own security memory mapping, then you should activate SAU in partition_stm32u5.h file (default SAU regions split are proposed in partition_stm32u5.h file, to be customized).
2024-01-14 08:11 AM
Okay, thank you so much for the quick response. Now it makes sense