cancel
Showing results for 
Search instead for 
Did you mean: 

How to Configure a Custom PHY Address inSTM32cube IDE 1.14.1?

priyazcs
Associate II

I'm using an STM32F427 and no RTOS, along with a custom PHY. However, I’ve encountered issues configuring a custom PHY address in STM32CubeIDE 1.14.1:

  1. Custom PHY Address Setup
    My setup requires a specific PHY address, such as 0x80, but STM32CubeIDE 1.14.1 only lists options for LAN8742 and DP83848. Selecting "Undefined PHY" triggers a warning, which limits proper configuration. In STM32CubeIDE 1.8.0, I was able to configure a custom PHY without any issues.

Could you please provide guidance on how to set up and configure a custom PHY in version 1.14.1? Any information on handling this in the latest versions to avoid warnings and allow for custom PHY addresses would be greatly appreciated.

Thank you.

1 REPLY 1
SofLit
ST Employee

Hello,

It's basically STM32CubeMx question and not STM32CubeIDE. The thread will be moved to STM32CubeMx forum board.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.