2021-05-08 02:28 AM
I have a Nucleo-H743ZI board and want to get the CDC example working so that I can use it in my own code.
I created a new STM32 Project from STMCubeIDE and selected the CDC Standalone example (It is for LUCLEO-L552ZE-Q board).
I had to disable BSP_LED_Init since it uses an I2C IO expander but rest of the code seems to be OK for the H743ZI board. There is sadly now response when I plug-in the USB port, so something still seems to be missing.
Any idea of what could be wrong and how can I fix it of how I can get the USB CDC example going on H743ZI board?
2021-05-11 07:39 AM
Hello @PWint ,
There is a "CDC-Standalone" application within STM32CubeH7 package and runs on STM32H743xx devices:
STM32Cube_FW_H7_V1.9.0\Projects\STM32H743I-EVAL\Applications\USB_Device\CDC_Standalone
You may update this working application according to your needs, and you find there a readme file describing how to use and run the example.
Hope my answer helped you! 😊
When your question is answered, please close this topic by choosing "Select as Best".
Imen
2021-05-11 11:29 AM
Hi @Imen DAHMEN,
Thank you very much for getting back to me. I did use the CDC-Standalone application but maybe my method is sending me down the wrong track.
I used STM32Cube to create a new example project:
1. File > New STM32 Project.
2. Under__Example Selector__ tab, in __Name__ field, type “CDC_Standalone�?.
3. Select “STM32H743I-EVAL�?.
4. Give project a name and press __Finish__.
5. When asked “Initialise all Peripherals with default Mode?�?, selected __Yes__.
This gives me a project for a different development board and strangely, it does not seem to have any CDC code in it. main.c initialises all the peripherals (almost all of which I do not need). Running this code on my platform predictably causes hard faults.
I’ve copied the folder from the example path you provided and then imported the STM32H743I-EVAL-FS project in STMCube. main.c in this code contains calls to USBD_RegisterClass() but I cannot build this project.
Should I be creating a new project from scratch and then manually pull in the code from the example project, or is there a simpler way that I am missing?
Regards,
PWInt
2021-05-17 01:41 AM
Hi @PWint ,
Sorry for the delayed reply on this, as I was on leave.
>> but I cannot build this project.
Do you get an error message ?
Did you checked the pin configuration ?
I suggest you to debug, localize where the code hangs and identify when the problem occurs.
Imen