2021-07-12 8:32 AM
2021-07-12 1:30 PM
Check/update the onboard STLink firmware.
https://community.st.com/s/question/0D50X00009XkeTwSAJ/stm32f4-disc1-reset-issue
JW
2021-07-12 1:49 PM
If there is a solder-bridge for NRST, consider removing that.
2021-07-18 12:53 PM
Hi Jan, hi Tesla,
thank you for ur answers.
The Problem is solved. Indeed there is a solid bridge between NRST and the on-board-developer (Pin T_NRST) at the buttom side.
I dont understand such a design because in such a case i await a jumper.
To close the SB again its fortunately possible to connect both pins on connectors at the top side.
:grinning_face: