2020-02-09 3:24 AM
why does this work:
HAL_UART_Transmit_DMA(&huart6, (uint8_t *)"stm32\n", 6); // works and sends data
and this doesnt:
ALIGN_32BYTES (uint8_t aTxBuffer[]) = "stm32\n";
HAL_UART_Transmit_DMA(&huart6, (uint8_t *)aTxBuffer, 6) // doesnt send any data
what am i missing?
Solved! Go to Solution.
2020-02-09 4:36 AM
solved! appreciate the quick responses, thank you!
for anyone whose reading this and having the same issue: this is what you're looking for https://community.st.com/s/article/FAQ-DMA-is-not-working-on-STM32H7-devices
2020-02-09 3:49 AM
Most likely aTxBuffer is located in DTCM, to which only the MDMA has access in H7 series. Take a look at AN4891 figure 1.
2020-02-09 3:51 AM
DMA buffers must be located in (the appropriate) RAM. Fixed strings or other constant data are usually stored in ROM (flash).
You should verify/ensure that the data is provided on stack / RAM.
2020-02-09 4:36 AM
solved! appreciate the quick responses, thank you!
for anyone whose reading this and having the same issue: this is what you're looking for https://community.st.com/s/article/FAQ-DMA-is-not-working-on-STM32H7-devices
2020-02-24 5:30 AM
Glad to know that your question is answered. Please mark the article as helpful in this case.
Thanks
Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.