cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_UART_Receive_IT is not working

KaushikSTM32
Associate

Originally a reply in this thread - split as a separate question.


Hello 

My blocking mode is working with "HAL_UART_Receive(&huart4, temp, 1, 100);"

Nonblocking mode is not working

Can you suggest anything to check?

I have defined as said

 

/* USER CODE BEGIN 2 */

HAL_UART_Receive_IT(&huart4, temp, 1);

/* USER CODE END 2 */

 

and

 

/* USER CODE BEGIN 4 */

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
  HAL_UART_Receive_IT(&huart4, temp, 1);
  HAL_UART_Transmit(&huart4, temp, 1, 100);
}

/* USER CODE END 4 */

 

29 REPLIES 29

Thank you so much sir,

I had signed off for today. I will confirm whether the above logic is working or not, tomorrow.

 

You still haven't indicated if you enabled the NVIC as suggested in a previous reply?

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
KaushikSTM32
Associate

sir,

Implemented and rechecked in blocking mode, Its working fine.

But facing the same problem with non blocking interrupt mode: when I entered a thing on serial terminal(putty) it got hanged and stopped my toggling also. code is attached.

 

/* USER CODE BEGIN Header */

/**

******************************************************************************

* @file : main.c

* @brief : Main program body

******************************************************************************

* @attention

*

* Copyright (c) 2025 STMicroelectronics.

* All rights reserved.

*

* This software is licensed under terms that can be found in the LICENSE file

* in the root directory of this software component.

* If no LICENSE file comes with this software, it is provided AS-IS.

*

******************************************************************************

*/

/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/

#include "main.h"

 

/* Private includes ----------------------------------------------------------*/

/* USER CODE BEGIN Includes */

 

/* USER CODE END Includes */

 

/* Private typedef -----------------------------------------------------------*/

/* USER CODE BEGIN PTD */

 

/* USER CODE END PTD */

 

/* Private define ------------------------------------------------------------*/

/* USER CODE BEGIN PD */

uint8_t UART4_rxBuffer[12] = {0};

/* USER CODE END PD */

 

/* Private macro -------------------------------------------------------------*/

/* USER CODE BEGIN PM */

 

/* USER CODE END PM */

 

/* Private variables ---------------------------------------------------------*/

UART_HandleTypeDef huart4;

unsigned char RXcplt;

/* USER CODE BEGIN PV */

 

/* USER CODE END PV */

 

/* Private function prototypes -----------------------------------------------*/

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

static void MX_UART4_Init(void);

/* USER CODE BEGIN PFP */

 

/* USER CODE END PFP */

 

/* Private user code ---------------------------------------------------------*/

/* USER CODE BEGIN 0 */

 

/* USER CODE END 0 */

 

/**

* @brief The application entry point.

* @retval int

*/

int main(void)

{

 

/* USER CODE BEGIN 1 */

 

/* USER CODE END 1 */

 

/* MCU Configuration--------------------------------------------------------*/

 

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */

HAL_Init();

 

/* USER CODE BEGIN Init */

 

/* USER CODE END Init */

 

/* Configure the system clock */

SystemClock_Config();

 

/* USER CODE BEGIN SysInit */

 

/* USER CODE END SysInit */

 

/* Initialize all configured peripherals */

MX_GPIO_Init();

MX_UART4_Init();

/* USER CODE BEGIN 2 */

HAL_UART_Receive_IT (&huart4, UART4_rxBuffer, 5);

RXcplt = 0;

/* USER CODE END 2 */

 

/* Infinite loop */

/* USER CODE BEGIN WHILE */

while (1)

{

/* USER CODE END WHILE */

// HAL_UART_Receive(&huart4, UART4_rxBuffer, 5, 1000);

// HAL_UART_Transmit(&huart4, UART4_rxBuffer, 5, 1000);

if(RXcplt)

{

RXcplt = 0;

HAL_UART_Transmit(&huart4, UART4_rxBuffer, 5, 1000);

HAL_UART_Receive_IT(&huart4, UART4_rxBuffer, 5);

}

HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_4);

HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);

/* USER CODE BEGIN 3 */

}

/* USER CODE END 3 */

}

 

/**

* @brief System Clock Configuration

* @retval None

*/

void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct = {0};

RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 

/** Configure the main internal regulator output voltage

*/

HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);

 

/** Initializes the RCC Oscillators according to the specified parameters

* in the RCC_OscInitTypeDef structure.

*/

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

RCC_OscInitStruct.HSIState = RCC_HSI_ON;

RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV4;

RCC_OscInitStruct.PLL.PLLN = 75;

RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;

RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;

RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

Error_Handler();

}

 

/** Initializes the CPU, AHB and APB buses clocks

*/

RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)

{

Error_Handler();

}

}

 

/**

* @brief UART4 Initialization Function

* @PAram None

* @retval None

*/

static void MX_UART4_Init(void)

{

 

/* USER CODE BEGIN UART4_Init 0 */

 

/* USER CODE END UART4_Init 0 */

 

/* USER CODE BEGIN UART4_Init 1 */

 

/* USER CODE END UART4_Init 1 */

huart4.Instance = UART4;

huart4.Init.BaudRate = 115200;

huart4.Init.WordLength = UART_WORDLENGTH_8B;

huart4.Init.StopBits = UART_STOPBITS_1;

huart4.Init.Parity = UART_PARITY_NONE;

huart4.Init.Mode = UART_MODE_TX_RX;

huart4.Init.HwFlowCtl = UART_HWCONTROL_NONE;

huart4.Init.OverSampling = UART_OVERSAMPLING_16;

huart4.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;

huart4.Init.ClockPrescaler = UART_PRESCALER_DIV1;

huart4.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;

if (HAL_UART_Init(&huart4) != HAL_OK)

{

Error_Handler();

}

if (HAL_UARTEx_SetTxFifoThreshold(&huart4, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)

{

Error_Handler();

}

if (HAL_UARTEx_SetRxFifoThreshold(&huart4, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)

{

Error_Handler();

}

if (HAL_UARTEx_DisableFifoMode(&huart4) != HAL_OK)

{

Error_Handler();

}

/* USER CODE BEGIN UART4_Init 2 */

 

/* USER CODE END UART4_Init 2 */

 

}

 

/**

* @brief GPIO Initialization Function

* @PAram None

* @retval None

*/

static void MX_GPIO_Init(void)

{

GPIO_InitTypeDef GPIO_InitStruct = {0};

/* USER CODE BEGIN MX_GPIO_Init_1 */

/* USER CODE END MX_GPIO_Init_1 */

 

/* GPIO Ports Clock Enable */

__HAL_RCC_GPIOA_CLK_ENABLE();

__HAL_RCC_GPIOC_CLK_ENABLE();

 

/*Configure GPIO pin Output Level */

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4|GPIO_PIN_5, GPIO_PIN_RESET);

 

/*Configure GPIO pins : PA4 PA5 */

GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5;

GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 

/* USER CODE BEGIN MX_GPIO_Init_2 */

/* USER CODE END MX_GPIO_Init_2 */

}

 

/* USER CODE BEGIN 4 */

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)

{

RXcplt = 1;

}

/* USER CODE END 4 */

 

/**

* @brief This function is executed in case of error occurrence.

* @retval None

*/

void Error_Handler(void)

{

/* USER CODE BEGIN Error_Handler_Debug */

/* User can add his own implementation to report the HAL error return state */

__disable_irq();

while (1)

{

}

/* USER CODE END Error_Handler_Debug */

}

 

#ifdef USE_FULL_ASSERT

/**

* @brief Reports the name of the source file and the source line number

* where the assert_param error has occurred.

* @PAram file: pointer to the source file name

* @PAram line: assert_param error line source number

* @retval None

*/

void assert_failed(uint8_t *file, uint32_t line)

{

/* USER CODE BEGIN 6 */

/* User can add his own implementation to report the file name and line number,

ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */

/* USER CODE END 6 */

}

#endif /* USE_FULL_ASSERT */
 

Yes Sir, this one?

Screen shot

uart.png

Attach your IOC file

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
KaushikSTM32
Associate

Yes sir, file is attached.

Hello @KaushikSTM32 

Please try to execute the code without transmit first. 

Could you share the content of status register before performing the second receive? Could you share the state of the handle and error code after finishing the first receive.

Could you please share the content of status register when getting stack? 

Could you indicate the STM32 MCU series you are working on please? 

I added a check of errors in your code when calling HAL UART API. Please see it below.

if(HAL_UART_Receive_IT (&huart4, UART4_rxBuffer, 5)!= HAL_OK)
  {
    Error_Handler();
  }

RXcplt = 0;

/* USER CODE END 2 */

 

/* Infinite loop */

/* USER CODE BEGIN WHILE */

while (1)

{

/* USER CODE END WHILE */

// HAL_UART_Receive(&huart4, UART4_rxBuffer, 5, 1000);

// HAL_UART_Transmit(&huart4, UART4_rxBuffer, 5, 1000);

if(RXcplt)

{

RXcplt = 0;

if(HAL_UART_Transmit(&huart4, UART4_rxBuffer, 5, 1000)!= HAL_OK)
  {
    Error_Handler();
  }

if(HAL_UART_Receive_IT(&huart4, UART4_rxBuffer, 5)!= HAL_OK)
  {
    Error_Handler();
  }

}


 

If your question is answered, please close this topic by clicking "Accept as Solution".

Thanks
Omar

Hello Sir,

Please try to execute the code without transmit first. 

* Same thing Toggling stopped.

Could you share the content of status register before performing the second receive? Could you share the state of the handle and error code after finishing the first receive.

Could you please share the content of status register when getting stack? 

*I am new to ST. Can you please provide the material to do that?

Could you indicate the STM32 MCU series you are working on please? 

* STM32G474VET6

 

I added a check of errors in your code when calling HAL UART API. Please see it below.

* Implemented the code

 

Sir,

It is getting reached at some infinite loop even my main while loop is not working after the first receive event.

 


@KaushikSTM32 wrote:

It is getting reached at some infinite loop 


What "infinite loop", exactly ?

This one, perhaps?

 

/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
   /* USER CODE BEGIN Error_Handler_Debug */
   /* User can add his own implementation to report the HAL error return state */

   __disable_irq();
   while (1)
   {
   }
   /* USER CODE END Error_Handler_Debug */
}

 

Or the Hard Fault handler?