2017-04-19 2:49 AM
Hello,
I have simple interfacing of STM32F0R8T6 with M24C01 EEPROM. It's been one week I am trying to read from EEPROM but buffer is responding with 0xFF value. My program successfully write values on EEPROM but fails to read them.
My function call:
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_I2C1_Init();uint8_t tab_write[3]= {1,2,3};uint8_t tab_read[3];
HAL_I2C_Master_Transmit(&hi2c1, 0xA0, tab_write, 3, 1000); // device address = 0xA0
HAL_I2C_Master_Receive(&hi2c1, 0xA0, tab_read, 3, 1000);
static void MX_I2C1_Init(void)
{hi2c1.Instance = I2C1;
hi2c1.Init.Timing = 0x50330309; // 400 Khz hi2c1.Init.OwnAddress1 = 0; hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE; hi2c1.Init.OwnAddress2 = 0; hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK; hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE; hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;}
I checked some tutorials as well as examples provided by ST by seeing them this code should work but it is not working.
When I use Error_Handler() for both functions it enters error handler of Receive function.
Am I missing something?
Thank you for comments.
#eeprom #stm32f0-i2c #hal_i2c_master_receiveSolved! Go to Solution.
2017-04-19 5:46 AM
not sure how you got the address A0 to work at all. HAL wants left justified address.
uint16_t mem_read_reg(uint16_t register_pointer)
{ HAL_StatusTypeDef status = HAL_OK; uint16_t return_value = 0;while (HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(0x50<<1), 3, 100) != HAL_OK) {}
status = HAL_I2C_Mem_Read(&hi2c1, // i2c handle
(uint16_t)(0x50<<1), // i2c address, left aligned (uint16_t)register_pointer, // register address I2C_MEMADD_SIZE_16BIT, // eeprom uses 16-bit register addresses &return_value, // place to put returned value 1, // return one byte 100); // timeout/* Check the communication status */
if(status != HAL_OK) {}
return return_value;
}2017-04-19 5:46 AM
not sure how you got the address A0 to work at all. HAL wants left justified address.
uint16_t mem_read_reg(uint16_t register_pointer)
{ HAL_StatusTypeDef status = HAL_OK; uint16_t return_value = 0;while (HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(0x50<<1), 3, 100) != HAL_OK) {}
status = HAL_I2C_Mem_Read(&hi2c1, // i2c handle
(uint16_t)(0x50<<1), // i2c address, left aligned (uint16_t)register_pointer, // register address I2C_MEMADD_SIZE_16BIT, // eeprom uses 16-bit register addresses &return_value, // place to put returned value 1, // return one byte 100); // timeout/* Check the communication status */
if(status != HAL_OK) {}
return return_value;
}2017-04-19 6:28 AM
In your example, you are writing @01=02 and @02=03 as the byte written after writing the slave write adr is the eep sub adr location. After write, wait 10msec, do a start a0 01 to ask readinf from location 01, then read 2 bytes by S a1.a xx.a xx.n P content read should be 02 and 03
2017-04-19 8:42 AM
Thank you for your precious reply. I didn't have idea about this. As writing operation was accepting 0xA0 as a device address I didn't think about aligning address to left. Now its working.