cancel
Showing results for 
Search instead for 
Did you mean: 

FreeRTOS + TCP in STM32Cube

Posted on August 05, 2015 at 20:57

Are there any plans to integrate the FreeRTOS + TCP into STM32Cube?  this would make the LwIP thread aware.  FreeRTOS has the basics but not completed for the STM32 so the level of effort would be moderate but probably well worth the time for STM.

thanks

#freertos+tcp
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on August 19, 2015 at 12:05

Hi craig,

Unfortunately, there is no plan for the moment to migrate to the FreeRTOS + TCP solution.

We already support the LwIP stack into the STM32Cube solution and it comes mainly with the same features as FreeRTOS + TCP.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.