cancel
Showing results for 
Search instead for 
Did you mean: 

Bug in HAL_RCC_GetSysClockFreq() / STM32Cube_FW_L1_V1.3.0 ?

tomtom9197
Associate II
Posted on August 18, 2015 at 15:20

I think I found a bug in STM32CubeL1 in function

HAL_RCC_GetSysClockFreq(). Clock settings are:

&sharpdefine HSE_VALUE    ((uint32_t)12000000) // external oscillator at 12 MHz

/* Enable HSE Oscillator and Activate PLL with HSE as source */

    RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

    RCC_OscInitStruct.HSEState = RCC_HSE_ON;

    RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

    RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

    RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL8;    //RCC_PLL_MUL12;

    RCC_OscInitStruct.PLL.PLLDIV = RCC_PLL_DIV3;

    if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {

        Error_Handler();

    }

/* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2

     clocks dividers */

    RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK

            | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);

    RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

    RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

    RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

    RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

    if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK) {

        Error_Handler();

    }

So I expected a SystemCoreClock = 32000000. But instead HAL_RCC_GetSysClockFreq() returned 24000000. It turns out that parentheses are wrong in the following section of HAL_RCC_GetSysClockFreq():

/* HSE used as PLL clock source */

pllvco = HSE_VALUE * (pllm / plld); // HSE_VALUE = 12000000, pllm = 8, plld = 3

After changing into

pllvco = (HSE_VALUE * pllm) / plld;

it returns 32000000 as expected.

This is because in the incorrect version above 8/3=2,6666 and the remainder is dropped, so 12MHz*2=24MHz!

#stm32cubel1
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on August 19, 2015 at 11:03

Hi sciro,

Thanks for your feedback. The issue has been reported internally.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.