2020-02-21 12:42 AM
I think on definition of Limit 3 is a error in the firmwarelibrary
Both OR are the same values.
#define LL_ADC_MULTI_REG_DMA_EACH_ADC 0x00000000U
#define LL_ADC_MULTI_REG_DMA_LIMIT_1 ( ADC_CCR_DMA_0)
#define LL_ADC_MULTI_REG_DMA_LIMIT_2 ( ADC_CCR_DMA_1 )
#define LL_ADC_MULTI_REG_DMA_LIMIT_3 ( ADC_CCR_DMA_0 | ADC_CCR_DMA_0)
#define LL_ADC_MULTI_REG_DMA_UNLMT_1 (ADC_CCR_DDS | ADC_CCR_DMA_0)
#define LL_ADC_MULTI_REG_DMA_UNLMT_2 (ADC_CCR_DDS | ADC_CCR_DMA_1 )
#define LL_ADC_MULTI_REG_DMA_UNLMT_3 (ADC_CCR_DDS | ADC_CCR_DMA_0 | ADC_CCR_DMA_0) Datasheet says
Bits 15:14 DMA: Direct memory access mode for multi ADC mode
This bit-field is set and cleared by software. Refer to the DMA controller section for more
details.
00: DMA mode disabled
01: DMA mode 1 enabled (2 / 3 half-words one by one - 1 then 2 then 3)
10: DMA mode 2 enabled (2 / 3 half-words by pairs - 2&1 then 1&3 then 3&2)
11: DMA mode 3 enabled (2 / 3 bytes by pairs - 2&1 then 1&3 then 3&2)
2020-02-26 7:31 AM
Hello,
You are right, I confirm this issue and we will fix it and verify if there is other impacted series.
In fact, the define in the stm32f4xx_ll_adc.h for "LL_ADC_MULTI_REG_DMA_LIMIT_3" and "LL_ADC_MULTI_REG_DMA_UNLMT_3" should be:
#define LL_ADC_MULTI_REG_DMA_LIMIT_3 ( ADC_CCR_DMA_1 | ADC_CCR_DMA_0)
#define LL_ADC_MULTI_REG_DMA_UNLMT_3 (ADC_CCR_DDS | ADC_CCR_DMA_1 | ADC_CCR_DMA_0)instead of:
#define LL_ADC_MULTI_REG_DMA_LIMIT_3 ( ADC_CCR_DMA_0 | ADC_CCR_DMA_0)
#define LL_ADC_MULTI_REG_DMA_UNLMT_3 (ADC_CCR_DDS | ADC_CCR_DMA_0 | ADC_CCR_DMA_0)Thank you for your contribution and highlighting this.
Best Regards,
Imen