2020-02-24 6:39 PM
Currently the STM32_L4 HAL provides HAL_UART_DMAPause and HAL_UART_DMAResume. These pause/resume both TX and RX on the UART.
I am using DMA for both transmit and receive on a UART. I have a case where I need to pause the receive (for flow control) but must still continue to transmit. It would be desirable to have this feature available in the HAL. For now I have resorted to copying the HAL_UART_DMAPause & HAL_UART_DMAResume code and removing the TX bits to make it work for my needs.
2020-02-25 12:08 AM
Hi @Rob.Riggs
Thanks for the input. I take note of the request.
I will check what could be done to serve it in future versions of HAL.
Regards
Guenael
2020-02-25 3:22 AM
I generally don't recommend to suspend DMA, unless you like inexplicable data loss
https://community.st.com/s/feed/0D50X00009XkW5oSAF
I know the above thread is 'F4 specific and I am aware of the fact that the 'L4 uses a different model of the DMA controller (1-port, vs. the 2-port DMA of 'F4); so this is more warning to the ST Cube coders, who already added these functions into 'F4 (and other Cubes) too.
JW