2021-07-15 5:56 AM
I tried to implement the USB and SDCard in a single project. but I am facing some problems as mentioned below,
Below is my microcontroller configuration:
Controller: stm32h743bit6
SYSCLK frequency: 480MHz
APB1 &2: 120MHz
TO SDMMC1,2: check from 8Mhz to 52MHz
TO USB: 48MHz
· Minimum Heap 0x400 / Minimum Stack 0x800
* USB and SDCard are working fine in the separate project configurations.
* But when integrated USB and SDCard in a single project facing some issues
- The read and write functions of USB and SDCard are working fine when both devices are connected to the controller(Without ejecting SDCard or USB from the controller board).
* When we remove sd card or USB in between operations, the below error is observed
- f_open or fmount functions will always return the FR_DISK_ERR .
- Once i get disk error, i cant perform any operation like read or writing data to usb or sd card
- Some times the code will be stopped the execution.
2021-08-31 2:06 AM
Hello @MB.9 ,
Take a look at the following example that shows how to use FatFS multi-drive: (Path : Projects\STM32F769I_EVAL\Applications\FatFs\FatFs_MultiDrives)
as well, take a look at this discussion that might be useful to you : STM32CubeMX Multi-Drive Support with FatFS
Otherwise, how error handling is done in your application?
BeST Regards,
Walid
2021-09-16 2:49 AM
Hello @MB.9 ,
Is there any news about your problem? Do you still have the same issues?
BeSt Regards,
Walid