2019-09-28 12:04 AM
I'm trying to use DMA in circular mode to modify the duty cycle of a PWM output. Ultimately, I plan to use it to communicate with WS2812B chips (like others have done with the STM32F4 chips). However, in my early tests I've noticed that it seems to send two pulses per buffer value.
For a simple example (full code at the end):
#define BUFFER_SIZE 2
uint16_t buffer[BUFFER_SIZE];
buffer[0] = htim3.Init.Period * .5; // 50%
buffer[1] = htim3.Init.Period * .9; // 90%
HAL_TIM_PWM_Start_DMA(&htim3, TIM_CHANNEL_1, (uint32_t*)buffer, BUFFER_SIZE);
There are 2 items in the buffer, one set at 50% duty cycle and the other at 90%. When circular mode is enabled, I would expect to see the PWM pulse to be alternating between the two. However, I see 2 pulses at 50% followed by 2 at 90%, and so on.
I'm sure I'm missing something elementary here. How do I get the pulses to alternate 50%, 90%, 50%, etc?
One of my thoughts was that the duplication could be caused by data width conversion on the data bus, as explained in section 11.3.4, page 268, of the reference manual (i.e. 16-bit value on a 32-bit bus) However, changing the DMA Data Alignment values doesn't change this.
Any ideas? Here's the code, which is based on the boiler plate created by STM32Cube:
#include <stdint.h>
#include "main.h"
#define SIGNAL_HZ 800000 // 800kHz
#define BUFFER_SIZE 2
TIM_HandleTypeDef htim3;
DMA_HandleTypeDef hdma_tim3_ch1;
uint16_t buffer[BUFFER_SIZE];
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_TIM3_Init(void);
static void MX_DMA_Init(void);
/**
* @brief The application entry point.
* @retval int
*/
int main(void) {
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_DMA_Init();
MX_TIM3_Init();
// PWM Buffer
buffer[0] = htim3.Init.Period * .5; // 50%
buffer[1] = htim3.Init.Period * .9; // 90%
// Start DMA -> PWM
HAL_TIM_PWM_Start_DMA(&htim3, TIM_CHANNEL_1, (uint32_t*)buffer, BUFFER_SIZE);
while (1) { }
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
// Oscillator init config
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLLMUL_4;
RCC_OscInitStruct.PLL.PLLDIV = RCC_PLLDIV_2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {
Error_Handler();
}
// Clock init config
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK) {
Error_Handler();
}
}
/**
* @brief TIM3 Initialization Function
* @param None
* @retval None
*/
static void MX_TIM3_Init(void) {
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
__HAL_RCC_TIM3_CLK_ENABLE();
htim3.Instance = TIM3;
htim3.Init.Prescaler = 0;
htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
htim3.Init.Period = (SystemCoreClock / SIGNAL_HZ) - 1;
htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_PWM_Init(&htim3) != HAL_OK) {
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK) {
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 0;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_ENABLE;
if (HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_1) != HAL_OK) {
Error_Handler();
}
if (HAL_TIMEx_RemapConfig(&htim3, TIM3_TI1_GPIO) != HAL_OK) {
Error_Handler();
}
}
/**
* Enable DMA controller clock
*/
static void MX_DMA_Init(void){
__HAL_RCC_DMA1_CLK_ENABLE();
hdma_tim3_ch1.Instance = DMA1_Channel5;
hdma_tim3_ch1.Init.Request = DMA_REQUEST_10;
hdma_tim3_ch1.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_tim3_ch1.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_tim3_ch1.Init.MemInc = DMA_MINC_ENABLE;
hdma_tim3_ch1.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD; // 16-bit PWM, but 32-bit bus
hdma_tim3_ch1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
hdma_tim3_ch1.Init.Mode = DMA_CIRCULAR;
hdma_tim3_ch1.Init.Priority = DMA_PRIORITY_LOW;
if (HAL_DMA_Init(&hdma_tim3_ch1) != HAL_OK) {
Error_Handler();
}
__HAL_LINKDMA(&htim3, hdma[TIM_DMA_ID_CC1], hdma_tim3_ch1);
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void) {
GPIO_InitTypeDef GPIO_PWMStruct = {0};
__HAL_RCC_GPIOA_CLK_ENABLE();
// PWM output pin - PA6
GPIO_PWMStruct.Pin = GPIO_PIN_6;
GPIO_PWMStruct.Mode = GPIO_MODE_AF_PP;
GPIO_PWMStruct.Pull = GPIO_PULLDOWN;
GPIO_PWMStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_PWMStruct.Alternate = GPIO_AF2_TIM3;
HAL_GPIO_Init(GPIOA, &GPIO_PWMStruct);
}
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void) {
}
Solved! Go to Solution.
2019-09-30 12:43 PM
The problem is a combination of
I've made this back of the envelope drawing, but these things tend to get much clearer if *you* make this or similar drawing:
The remedy is simple, don't trigger DMA from CC, but from Update, i.e. don't set TIMx_DIER.CC1DE, but TIMx_DIER.UDE.
It maybe will then also be a different channel in DMA and different setting in its triggers-inputs-mux, look it up in the DMA chapter).
I don't Cube.
JW
2019-09-28 2:46 AM
I am honestly puzzled.
Read out and post the content of relevant DMA and TIM registers.
JW
2019-09-30 9:54 AM
Some register values and a few more thoughts/questions:
Some of the TIM3 registers, using GDB:
I paused the application several times and can confirm the correct number is being set to CCR1. I cannot track the the value in real-time, since it's being transferred outside of CPU operations.
I'm not sure which DMA registers would help us here, but here are some of them:
I'm new to DMA, so I'd love to check my assumptions from what I've read about how this should work...
When setting DMA to memory -> peripheral (TIM). As I understand it, the peripheral (TIM3, in this case) will make a request to the DMA controller to receive the next value from memory. DMA will then send the value and, in this case, increment the memory location pointer for the next request.
Assumptions/Questions:
It almost seems like a timer repetition counter is set to 2, but from what I can tell the STM32l0xx doesn't have a repetition counter.
The next thing I'm going to try is using the transfer complete flag in the DMA interrupt to toggle an output pin and see how that lines up with the other signal on the scope. That won't tell me a lot, but it might give me another piece of information.
2019-09-30 12:42 PM
Another thought. Looking at the timer registers, DIER has UDE (bit 8 - Update DMA request enable) set to 0. This could be affecting the request event, even though tthe CC1DE (bit 9 - Capture/Compare 1 DMA request enable) is enabled.
2019-09-30 12:43 PM
The problem is a combination of
I've made this back of the envelope drawing, but these things tend to get much clearer if *you* make this or similar drawing:
The remedy is simple, don't trigger DMA from CC, but from Update, i.e. don't set TIMx_DIER.CC1DE, but TIMx_DIER.UDE.
It maybe will then also be a different channel in DMA and different setting in its triggers-inputs-mux, look it up in the DMA chapter).
I don't Cube.
JW
2019-09-30 1:13 PM
Wow, thank you for such a thorough response -- this is very helpful! I will give this a try tonight.
(I'm also starting to look at moving off of Cube)
2019-10-01 12:23 PM
It worked! Thanks again for the explanation.
For anyone else stumbling on this thread:
// Enable the update request DMA event
SET_BIT(TIM3->DIER, TIM_DIER_UDE);
// Disable capture/compare DMA event
CLEAR_BIT(TIM3->DIER, TIM_DIER_CC1DE);
If using HAL_TIM_PWM_Start_DMA, these lines need to come after that.