cancel
Showing results for 
Search instead for 
Did you mean: 

Check on wake up reason after interrupt by RTC timer or interrupt pin

hlmn7
Associate II

I do have problem to check wake up flag after wake-up from RTC timer or interrupt pin. This is my code block to check flag after wake-up:

 

 

void InitiateMode(int timeValue) { turnOffPeripherals(); timeValue = getTimeValue(timeValue); printf("\ngetMilSecBInSecond : %d\ntimeValue : %d\n\n", getMilSecBInSecond(), timeValue); HAL_SuspendTick(); HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, timeValue, RTC_WAKEUPCLOCK_CK_SPRE_16BITS); printf("Boot : "); printf("%d\n", bootCount); printf("Sleep mode Start\n"); printf("Enable deep sleep, Will wake up in %d seconds\n\n", timeValue); /* Enter STOP 2 mode */ // HAL_PWREx_EnterSTOP0Mode(PWR_STOPENTRY_WFI); // HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI); getTotalTime(); // betol2 sebelom HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI); printf(" 2\n"); // Check RTC Wake-Up Timer Flag if (__HAL_RTC_WAKEUPTIMER_GET_FLAG(&hrtc, RTC_FLAG_WUTF) != RESET) { // Wake-up event detected, clear the flag __HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF); // Your code to turn on the LED or perform other actions printf("Wake-up event detected by RTC timer, clear the flag\n"); } if(__HAL_GPIO_EXTI_GET_FLAG(GPIO_PIN_7) != RESET) { // Wake-up event detected, clear the flag __HAL_GPIO_EXTI_CLEAR_FLAG(GPIO_PIN_7); // Your code to turn on the LED or perform other actions printf("Wake-up event detected by interrupt pin, clear the flag\n"); } HAL_RTCEx_DeactivateWakeUpTimer(&hrtc); SystemClock_Config(); // processable start hidup sini // printf("\nBetol 2 lepas wake up : %d\n", HAL_GetTick()); printf("\nBetol 2 lepas wake up : %lu\n", HAL_GetTick()); HAL_ResumeTick(); getTickTimeStart(); printf("Sleep mode End\n"); printf("Wake Up!!\n"); printf("----------------------------------------------------------------\n\n"); // Increment the bootCount ++bootCount; printf("Bootcount : %d\n", bootCount); }
View more

 

The section:

 

// Check RTC Wake-Up Timer Flag if (__HAL_RTC_WAKEUPTIMER_GET_FLAG(&hrtc, RTC_FLAG_WUTF) != RESET) { // Wake-up event detected, clear the flag __HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF); // Your code to turn on the LED or perform other actions printf("Wake-up event detected by RTC timer, clear the flag\n"); } // Check GPIO 7 interrupt pin Flag if(__HAL_GPIO_EXTI_GET_FLAG(GPIO_PIN_7) != RESET) { // Wake-up event detected, clear the flag __HAL_GPIO_EXTI_CLEAR_FLAG(GPIO_PIN_7); // Your code to turn on the LED or perform other actions printf("Wake-up event detected by interrupt pin, clear the flag\n"); }

 

I set 10 second timer during STOP2 mode, after that the system wake-up, but when i check the log, no line is printed mean that __HAL_RTC_WAKEUPTIMER_GET_FLAG(&hrtc, RTC_FLAG_WUTF) == RESET or __HAL_GPIO_EXTI_CLEAR_FLAG(GPIO_PIN_7) == RESET, is there any problem in my code? please help me sifu, i am already struck by lighting

 

3 REPLIES 3
Sarra.S
ST Employee

Hello @hlmn7

Could you check the initial state of flags before entering stop2 mode?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

hlmn7
Associate II

Thanks for the reply, I just checked the initial state with the code added in void InitiateMode below:

// Check RTC Wake-Up Timer Flag if (__HAL_RTC_WAKEUPTIMER_GET_FLAG(&hrtc, RTC_FLAG_WUTF) == SET) { // Your code to turn on the LED or perform other actions printf("Wake-up RTC timer flag is SET\n"); } else { printf("Wake-up RTC timer flag is RESET\n"); } // Check GPIO 7 interrupt pin Flag if (__HAL_GPIO_EXTI_GET_FLAG(GPIO_PIN_7) == SET) { // Your code to turn on the LED or perform other actions printf("Interrupt GPIO_PIN_7 flag is SET\n"); } else { printf("Interrupt GPIO_PIN_7 flag is RESET\n"); }

the output:

22:12:22:545 -> Total time process : 6119 22:12:22:545 -> Wake-up RTC timer flag is RESET 22:12:22:545 -> Interrupt GPIO_PIN_7 flag is RESET

both are in reset state like I taught on top of the topic, I have no idea what to do next, I really need help on this.
@Sarra.S 

Hi @Sarra.S, please check my latest reply. Thanks.