2018-04-25 12:05 PM
Hello,
I want to know if there is any way to reallocate a sensor configured on a pin from STM32F091VCx to another pin.
I have a wind direction sensor that originally was digital and had all the measurement, treatment and sending configuration but right now I needed to change it and it is analogic. However the pin that it was connected (PD0) does not have an ADC builted in so I must change the pin to one that does have the ADC. So, I want to know if there is any document or something like that I can use to 'give me a north' without need to rebuild all the project because it was from third partner and I'm kinda lost.
By the way, I'm using the IAR 7.70.1, generating a blank project with the STM32CubeMX and copy all the third-partner firmware files to the SRC folder and add on the IAR.
#embedded-firmware #hal-adc #adc-configuration2018-04-26 09:18 AM
Hi
vlqueiroz93
,You have to refer to the pinout table in
to know the ADC pins and select the suitable one to be configured in your case.As you are already generating a blank project with STM32CubeMX, you can also use it to configure an ADC channel and select the suitable pin for your application.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.