lwIp netconn API UDP connection
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-04-26 11:28 PM
Posted on April 27, 2018 at 08:28
please tell me more about UDP PORT:-
this is my code:-(Is it correct or not)
void StartDefaultTask(void const * argument)
{ /* init code for LWIP */ MX_LWIP_Init();/* USER CODE BEGIN 5 */
/* conn = netconn_new( NETCONN_UDP ); netconn_bind(conn,IP_ADDR_ANY, 7); //local portnetconn_connect(conn, IP_ADDR_BROADCAST, 1235 );
*/ conn = netconn_new(NETCONN_UDP);if(conn!=NULL){ HAL_UART_Transmit(&huart3,'new\r\n',5,100); HAL_Delay(100);} /* set up the IP address of the remote host */ addr.addr = htonl(0xC0A86472);/* connect the connection to the remote host */
if(netconn_bind(conn,&addr,55555)==ERR_OK) { HAL_UART_Transmit(&huart3,'bind\r\n',6,100); HAL_Delay(100); } if( netconn_connect(conn,&addr,0)==ERR_OK){ HAL_UART_Transmit(&huart3,'connect\r\n',9,100); HAL_Delay(100);} /* Infinite loop */ for(;;) { /* create a new netbuf */ HAL_UART_Transmit(&huart3,'default\r\n',9,100); HAL_Delay(100);buf = netbuf_new();
if(buf!=NULL){ HAL_UART_Transmit(&huart3,'netbuf_new\r\n',12,100); HAL_Delay(100);} data = netbuf_alloc(buf, 10);if(data!=NULL){ HAL_UART_Transmit(&huart3,'netbuf_alloc\r\n',14,100); HAL_Delay(100);} /* create some arbitrary data */ for(i = 0; i < 10; i++) data[i] = 'a';/* send the arbitrary data */
if(netconn_send(conn, buf)==ERR_OK) { HAL_UART_Transmit(&huart3,'sending1\r\n',10,100); HAL_Delay(100); }vTaskDelay( 200 ); //some delay! /* reference the text into the netbuf */ if(netbuf_ref(buf, text, sizeof(text))==ERR_OK) { HAL_UART_Transmit(&huart3,'netbuf_ref\r\n',12,100); HAL_Delay(100); }/* send the text */
if(netconn_sendto(conn,buf,&addr,55555)==ERR_OK) { HAL_UART_Transmit(&huart3,'sending2\r\n',10,100); HAL_Delay(100); } vTaskDelay( 200 ); //some delay! /* deallocate connection and netbuf */ netbuf_delete(buf); osDelay(1); } /* USER CODE END 5 */ }#lwip* #udp #netconn #freertos
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0