cancel
Showing results for 
Search instead for 
Did you mean: 

camera module for stm32

suman_99
Associate II

which camera module is used for stm32...?

1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hello @suman_99 and welcome to the STCommunity :),

To know if a CMOS sensor (a camera module) is compatible with the DCMI or not, the user must check the
following points in the CMOS sensor specifications:
• parallel interface (8-, 10-, 12-, or 14-bit)
• control signals (VSYNC, HSYNC, and PIXCLK)
• supported pixel clock frequency output
• supported data output

There is a wide range of camera modules and CMOS sensors that are compatible with the STM32 DCMI.
The table below lists some of them.

KDJEM1_0-1704803056462.png

Also you can  check in AN5020 table 6. some examples of DCMI and camera modules on STM32 boards.

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
KDJEM.1
ST Employee

Hello @suman_99 and welcome to the STCommunity :),

To know if a CMOS sensor (a camera module) is compatible with the DCMI or not, the user must check the
following points in the CMOS sensor specifications:
• parallel interface (8-, 10-, 12-, or 14-bit)
• control signals (VSYNC, HSYNC, and PIXCLK)
• supported pixel clock frequency output
• supported data output

There is a wide range of camera modules and CMOS sensors that are compatible with the STM32 DCMI.
The table below lists some of them.

KDJEM1_0-1704803056462.png

Also you can  check in AN5020 table 6. some examples of DCMI and camera modules on STM32 boards.

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

KDJEM.1
ST Employee

Hi @suman_99 ,

Does my reply answer you request ?

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi @KDJEM.1,

Thank you for your reply! but we need help discovering a suitable camera module for the STM32L496AG.

Specifications of the camera:

*compatible with the DCMI
*5MP rgb ir digital camera
*camera driver code support for STM32L496AG.

 

Thank you,

Suman.