2024-06-08 10:29 AM
STM32Cube FW_F4 V1.28
STM32CubeMX 6.11.1
file main.c line 209 function static void MX_SDIO_SD_Init(void)
hsd.Init.BusWide = SDIO_BUS_WIDE_4B;
fix
hsd.Init.BusWide = SDIO_BUS_WIDE_1B;
Related post.
Solved! Go to Solution.
2024-06-28 09:30 AM
No need to report it as it was already treated in https://community.st.com/t5/stm32cubemx-mcus/sdio-interface-not-working-in-4bits-with-stm32f4-firmware/m-p/591803#M26033 . and the internal ticket number 155983 was opened.
2024-06-10 01:28 AM
Hello,
Your comment is not clear. Do you mean that the solution proposed solution in https://community.st.com/t5/stm32cubemx-mcus/sdio-interface-not-working-in-4bits-with-stm32f4-firmware/td-p/591776 doesn't work?
2024-06-28 09:04 AM
Hi SofLit. I just reported bug for setup above and it can be fixed as proposed in post.
2024-06-28 09:30 AM
No need to report it as it was already treated in https://community.st.com/t5/stm32cubemx-mcus/sdio-interface-not-working-in-4bits-with-stm32f4-firmware/m-p/591803#M26033 . and the internal ticket number 155983 was opened.