cancel
Showing results for 
Search instead for 
Did you mean: 

[bug]STM32CubeMX incorrect clock configuration for Nucleo-F446ZE

thom_as
Associate II
Posted on May 24, 2016 at 17:04

The Nucleo-F446ZE use an STM32F446ZET6U

When I create a project for the nucleo, HSI is incorrect (HSI = 8Mhz but should be 16 Mhz)

If I choose the mcu only, the HSI value is correct.

#stm32f4 #stm32cube #bug
5 REPLIES 5
Nesrine M_O
Lead II
Posted on May 24, 2016 at 18:01

Hi none.thomas,

Please upgrade to latest CubeMX 4.15 release, the issue has been fixed.

Syrine-

thom_as
Associate II
Posted on May 25, 2016 at 09:23

I updated everything.

STM32Cube 4.0

STM32CubeF4 Firmware Package V1.0/ 06-may-2016

I uninstalled older firmware package and restarted the software but the error still here

Nesrine M_O
Lead II
Posted on May 25, 2016 at 11:29

Hi none.thomas,

You are using STM32F446 NUCLEO 144 but I do the test with a STM32F446 NUCLEO 64 where there is no problem.

I confirm your issue and I'll report it to our MX team for checking. Sorry for the inconvenience it may bring.

-Syrine-

pokezel
Associate
Posted on August 11, 2016 at 00:42

Sorry for bumping an old thread - has there been any update on this issue?

Currently experiencing it myself.

Sirma Siang
ST Employee
Posted on November 07, 2016 at 16:01

Hello Heilicher Ethan,

I thank you for your bug report.

You are absolutely right, and I confirm that this is solved in the next CubeMx release (4.18).

Kind Regards

Sirma