Behavior with _LOW_POWER
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-09 2:36 AM
Hi everyone,
I am working on an USB-PD source that is battery powered.
To make use of the low power features, I defined _LOW_POWER.
When this is defined, I get a problem in connection with eletronically marked cables (EMC). Non-EMC cables work fine.
The system will get stuck in the state currentHWcondition "HW_PwrCable_NoSink_Attachment".
I investigated the issue and found that the system works perfectly once I commented the following lines in usbpd_cad_hw_if.c related to _LOW_POWER
uint32_t CAD_StateMachine(uint8_t PortNum, USBPD_CAD_EVENT *pEvent, CCxPin_TypeDef *pCCXX)
{
CAD_HW_HandleTypeDef *_handle = &CAD_HW_Handles[PortNum];
uint32_t _timing = CAD_DEFAULT_TIME;
/* set by default event to none */
*pEvent = USBPD_CAD_EVENT_NONE;
if (USBPD_TRUE == Ports[PortNum].params->PE_SwapOngoing)
{
return _timing;
}
if (_handle->CAD_ErrorRecoveryflag == USBPD_TRUE)
{
/* Force the state error recovery */
_handle->CAD_ErrorRecoveryflag = USBPD_FALSE;
_handle->cstate = USBPD_CAD_STATE_ERRORRECOVERY;
#if defined(_TRACE)
USBPD_TRACE_Add(USBPD_TRACE_CAD_LOW, PortNum, (uint8_t)_handle->cstate, NULL, 0);
#endif /* _TRACE */
}
switch(_handle->cstate)
{
case USBPD_CAD_STATE_RESET:
{
//#if !defined(_LOW_POWER) && !defined(USBPDM1_VCC_FEATURE_ENABLED)
//DBG
LL_UCPD_EnableIT_TypeCEventCC2(Ports[PortNum].husbpd);
LL_UCPD_EnableIT_TypeCEventCC1(Ports[PortNum].husbpd);
//#endif /* !_LOW_POWER */
if( 0 == PortNum)
{
UCPD_INSTANCE0_ENABLEIRQ;
}
#if USBPD_PORT_COUNT > 1
else
{
UCPD_INSTANCE1_ENABLEIRQ;
}
#endif /* USBPD_PORT_COUNT > 1 */
#if defined(_DRP) || defined(_ACCESSORY_SNK)
_handle->CAD_tToggle_start = HAL_GetTick();
#endif /* _DRP || _ACCESSORY_SNK */
_handle->cstate = USBPD_CAD_STATE_DETACHED;
break;
}
void CAD_Check_HW_SRC(uint8_t PortNum)
{
#if !defined(_RTOS)
uint32_t CC1_value_temp, CC2_value_temp;
#endif /* !_RTOS */
CAD_HW_HandleTypeDef *_handle = &CAD_HW_Handles[PortNum];
/* done to prevent code optimization issue with GCC */
uint32_t CC1_value, CC2_value;
/*
----------------------------------------------------------------------------
| ANAMODE | ANASUBMODE[1:0] | Notes | TYPEC_VSTATE_CCx[1:0] |
| | | | 00 | 01 | 10 | 11 |
----------------------------------------------------------------------------
| 0: Source | 00: Disabled |Disabled N/A | NA |
| | 01: Default USB Rp| |vRaDef|vRdDef|vOPENDef| |
| | 10: 1.5A Rp | |vRa1.5|vRd1.5|vOPEN1.5| NA |
| | 11: 3.0A Rp | |vRa3.0|vRd3.0|vOPEN3.0| NA |
-----------------------------------------------------------------------------
| 1: Sink | | |xx vRa|vRdUSB| vRd1.5 |vRd3.0|
-----------------------------------------------------------------------------
*/
//DBG
//#ifdef _LOW_POWER
// /* Enable type C state machine */
// CLEAR_BIT(Ports[PortNum].husbpd->CR, UCPD_CR_CC1TCDIS | UCPD_CR_CC2TCDIS);
// for(int32_t index=0; index < 200/2; index++){ __DSB();};
//#endif /* _LOW_POWER */
CC1_value = (Ports[PortNum].husbpd->SR & UCPD_SR_TYPEC_VSTATE_CC1) >> UCPD_SR_TYPEC_VSTATE_CC1_Pos;
CC2_value = (Ports[PortNum].husbpd->SR & UCPD_SR_TYPEC_VSTATE_CC2) >> UCPD_SR_TYPEC_VSTATE_CC2_Pos;
//DBG
//#ifdef _LOW_POWER
// /* Disable the C state machine */
// SET_BIT(Ports[PortNum].husbpd->CR, UCPD_CR_CC1TCDIS | UCPD_CR_CC2TCDIS);
//#endif /* _LOW_POWER */
Is this a known issue or am I using the code wrong in some other place?
Thanks,
Christian
- Labels:
-
STM32G0 Series
-
USB-PD
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-09-26 11:39 PM
Dear Christian,
Is it possible to provide the project to this thread?
regards,
Yohann
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-10-14 4:03 AM
Dear Yohann,
yes I can share it with you. Is there any way I can get it to you?

- « Previous
-
- 1
- 2
- Next »