cancel
Showing results for 
Search instead for 
Did you mean: 

About the transfer function for the closed-loop system in AN5496

diverger
Senior

Hi, I'm reading the AN5496 - Rev 3. I'm confused by equation (6) and (7). If all they are the transfer function of the closed-loop system, why there are different?

Thanks.

2 REPLIES 2
FBL
ST Employee

Hello @diverger​,

Thank you for your contribution on ST Community,

I will check internally and get back to you soon.

The explanation may not be clear.

Thanks for highlighting it!

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

FBL
ST Employee

Hello @diverger​, 

The transfer function is not synthesized in terms of Hp(s), Hc(s) and PWM. It would be better to explain the closed loop transfer explicitly.

An internal ticket has been submitted.

Internal ticket number: 149070 (This is an internal tracking number and is not accessible or usable by customers).

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.