2024-05-13 6:24 AM - edited 2024-05-13 6:32 AM
Hi,
I am currently working on EMAC and I am a beginner ,So I want to know that why RX_ER is made optional for connection and if it made optional then how the errors are detected during reception.
@STea
2024-05-13 9:13 AM
As far as I understand: to off-load the STM32, and the STM32's RMII just doesn't do anything with it.
See this:
https://community.st.com/t5/stm32-mcus-products/ethernet-rmii-rx-error/td-p/440696
The link status should be checked regularly by reading the PHY registers.
When I look at the LAN8742 datasheet, it seems that RX_ER shows an error on the lowest hardware layer.
If that happens, there's some really bad things going on...