cancel
Showing results for 
Search instead for 
Did you mean: 

HELP UART HM10 dynamic size data receive

ISHA
Associate II

HELLO, 

i am new to STM, i am stuck in receiving dynamic size data from HM10 to stm32f407VG over UART2 communication , i tried  HAL_UART_Receive_IT(&huart2, &UART2_rxBuffer[rxIndex], 1); but not able to receive multiple char as 3rd part of this HAL_UART_Receive_IT(&huart2, &UART2_rxBuffer[rxIndex], 1); is 1 if i make it 12 then if i recive 12 char then data is visible and i want to receive any size of data string . 

please help

THANKS

 

/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * <h2><center>&copy; Copyright (c) 2024 STMicroelectronics.
  * All rights reserved.</center></h2>
  *
  * This software component is licensed by ST under BSD 3-Clause license,
  * the "License"; You may not use this file except in compliance with the
  * License. You may obtain a copy of the License at:
  *                        opensource.org/licenses/BSD-3-Clause
  *
  ******************************************************************************
  */
/* USER CODE END Header */
 
/* Includes ------------------------------------------------------------------*/
#include "main.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <string.h>
 
#include"liquidcrystal_i2c.h"
//#include "stdio.h"
 
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
 
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
I2C_HandleTypeDef hi2c1;
 
UART_HandleTypeDef huart2;
 
/* USER CODE BEGIN PV */
uint8_t UART2_rxBuffer[2] = {0};//should be 4 if sending isha
#define RX_BUFFER_SIZE 100
uint8_t data1Received = 0;
uint8_t data2Received = 0;
//#define RX_BUFFER_SIZE 50
//char rxBuffer[RX_BUFFER_SIZE];
//uint8_t rxIndex = 0;
//volatile uint8_t rxComplete = 0;
//#define LED12_PIN GPIO_PIN_12
//#define LED15_PIN GPIO_PIN_15
//char Rx_data[25] = "";
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_I2C1_Init(void);
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
//uint8_t Data[64];
//void Delay_ms(volatile int time_ms);
 
//void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t Size)
//{
// if (huart->Instance == USART2)
// {
// HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
// //HAL_UART_Transmit(&huart2, Data, Size, 1000);
// //HAL_UART_Transmit(&huart2, Data, Size, 1000);
// }
//// else if (huart2->Instance == USART2)
//// {
////
//// //HAL_UART_Transmit(&huart1, Data, Size, 1000);
//// }
// //HAL_UART_Receive_IT(huart2, Data, 64);
// HAL_UART_Receive_IT(huart, Data, 64);
//}
 
//void HAL_UART_ErrorCallback(UART_HandleTypeDef *huart)
//{
//    // Handle UART errors here
//    // Print error message on LCD
//    HD44780_Clear();
//    HD44780_SetCursor(0, 0);
//    HD44780_PrintStr("UART error");
//}
 
 
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
HAL_UART_Transmit(&huart2, UART2_rxBuffer, 2, 50);//
   // HAL_UART_Receive_IT(&huart2, UART2_rxBuffer, 2);//should be 4 if sending data
HD44780_Clear();
    HD44780_SetCursor(0,0);
    HD44780_PrintStr("gio");
    if (strncmp((char *)UART2_rxBuffer, "ON", 2) == 0)
            {
                // Turn on LED connected to pin 15
                HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);
    //data1Received = 1; // Set flag for "isha" received
    //data2Received = 0; // Clear flag for "jeet" received
            }
            // Check if "jeet" is received
            else if (strncmp((char *)UART2_rxBuffer, "OF", 2) == 0)
            {
                // Turn on LED connected to pin 14
            HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);
                //HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET); // ID if task is simple
            //data2Received = 1; // Set flag for "jeet" received// ID IF task is time taking
            //data1Received = 0; // Clear flag for "isha" received // ID IF task is time taking
            }
    if (huart->Instance == USART2)
    {
    HD44780_Clear();
    HD44780_SetCursor(0,0);
    HD44780_PrintStr("instance");
 
        //HD44780_Clear();
        HD44780_SetCursor(0, 1);
        HD44780_PrintStr("Received: ");
        HD44780_PrintStr((char *)UART2_rxBuffer);
 
    }
    HAL_UART_Receive_IT(&huart2, UART2_rxBuffer, 2);//should be 4 if sending data
}
 
//void toggleLEDs(void)
//{
//    // Toggle LED 15 if "isha" received
//    if (data1Received)
//    {
//        HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_15);
//    }
//
//    // Toggle LED 14 if "jeet" received
//    if (data2Received)
//    {
//        HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_14);
//    }
//}
 
/* USER CODE END 0 */
 
/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* USER CODE BEGIN 1 */
 
  /* USER CODE END 1 */
  
 
  /* MCU Configuration--------------------------------------------------------*/
 
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
 
  /* USER CODE BEGIN Init */
 
  /* USER CODE END Init */
 
  /* Configure the system clock */
  SystemClock_Config();
 
  /* USER CODE BEGIN SysInit */
 
  /* USER CODE END SysInit */
 
  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_USART2_UART_Init();
  MX_I2C1_Init();
  /* USER CODE BEGIN 2 */
  HAL_UART_Receive_IT (&huart2, UART2_rxBuffer, 2);
  HD44780_Init(2);
        HD44780_Clear();
        HD44780_SetCursor(0,0);
        HD44780_PrintStr("HELLO");
        HAL_Delay(200);
  /* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
//   toggleLEDs(); // Toggle LEDs based on received strings
//
//             // Delay for 500 milliseconds (0.5 second)
//             HAL_Delay(500);
//
//             // Repeat for a total of 6 times to create a 3-second toggle
//             for (int i = 0; i < 6; i++)
//             {
//                 toggleLEDs(); // Toggle LEDs based on received strings
//
//                 // Delay for 500 milliseconds (0.5 second)
//                 HAL_Delay(100);
//             }
//
//             // Clear the flags after 3 seconds
//           data1Received = 0;
//         data2Received = 0;
//      if (rxComplete) {
//          rxComplete = 0; // Reset flag
//
//          // Process received data
//          if (strcmp(rxBuffer, "hello") == 0) {
//              HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET); // Turn on LED12
//              HAL_Delay(1000); // Delay for 1 second
//              HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET); // Turn off LED12
//          }
//          else if (strcmp(rxBuffer, "hii") == 0) {
//              HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET); // Turn on LED15
//              HAL_Delay(1000); // Delay for 1 second
//              HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET); // Turn off LED15
//          }
//
//          // Clear the buffer
//          memset(rxBuffer, 0, sizeof(rxBuffer));
//          rxIndex = 0;
//
//          // Start another reception
//          HAL_UART_Receive_IT(&huart2, (uint8_t*)&rxBuffer[rxIndex], 1);
//      }
 
//   HAL_UART_Receive(&huart2,(uint8_t*)rxBuffer,RX_BUFFER_SIZE,100);
//   printf(" %s\n", rxBuffer);
//      if (strcmp(rxBuffer, "hello") == 0) {
//          HAL_GPIO_WritePin(GPIOD, LED12_PIN, GPIO_PIN_SET); // Turn on LED12
//          HAL_Delay(1000); // Delay for 1 second
//          HAL_GPIO_WritePin(GPIOD, LED12_PIN, GPIO_PIN_RESET); // Turn off LED12
//      }
//      else if (strcmp(rxBuffer, "hii") == 0) {
//          HAL_GPIO_WritePin(GPIOD, LED15_PIN, GPIO_PIN_SET); // Turn on LED15
//          HAL_Delay(1000); // Delay for 1 second
//          HAL_GPIO_WritePin(GPIOD, LED15_PIN, GPIO_PIN_RESET); // Turn off LED15
//      }
    /* USER CODE END WHILE */
 
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}
 
/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
  /** Configure the main internal regulator output voltage 
  */
  __HAL_RCC_PWR_CLK_ENABLE();
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
  /** Initializes the CPU, AHB and APB busses clocks 
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
  RCC_OscInitStruct.PLL.PLLM = 8;
  RCC_OscInitStruct.PLL.PLLN = 168;
  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
  RCC_OscInitStruct.PLL.PLLQ = 4;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
  /** Initializes the CPU, AHB and APB busses clocks 
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
 
  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
  {
    Error_Handler();
  }
}
 
/**
  * @brief I2C1 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_I2C1_Init(void)
{
 
  /* USER CODE BEGIN I2C1_Init 0 */
 
  /* USER CODE END I2C1_Init 0 */
 
  /* USER CODE BEGIN I2C1_Init 1 */
 
  /* USER CODE END I2C1_Init 1 */
  hi2c1.Instance = I2C1;
  hi2c1.Init.ClockSpeed = 100000;
  hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
  hi2c1.Init.OwnAddress1 = 0;
  hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
  hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
  hi2c1.Init.OwnAddress2 = 0;
  hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
  hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
  if (HAL_I2C_Init(&hi2c1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN I2C1_Init 2 */
 
  /* USER CODE END I2C1_Init 2 */
 
}
 
/**
  * @brief USART2 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_USART2_UART_Init(void)
{
 
  /* USER CODE BEGIN USART2_Init 0 */
 
  /* USER CODE END USART2_Init 0 */
 
  /* USER CODE BEGIN USART2_Init 1 */
 
  /* USER CODE END USART2_Init 1 */
  huart2.Instance = USART2;
  huart2.Init.BaudRate = 9600;
  huart2.Init.WordLength = UART_WORDLENGTH_8B;
  huart2.Init.StopBits = UART_STOPBITS_1;
  huart2.Init.Parity = UART_PARITY_NONE;
  huart2.Init.Mode = UART_MODE_TX_RX;
  huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart2.Init.OverSampling = UART_OVERSAMPLING_16;
  if (HAL_UART_Init(&huart2) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN USART2_Init 2 */
 
  /* USER CODE END USART2_Init 2 */
 
}
 
/**
  * @brief GPIO Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
 
  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOH_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOD_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();
 
  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15, GPIO_PIN_RESET);
 
  /*Configure GPIO pins : PD12 PD13 PD14 PD15 */
  GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
 
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
 
  /* USER CODE END Error_Handler_Debug */
}
 
#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @PAram  file: pointer to the source file name
  * @PAram  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

 

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Karl Yamashita
Principal

Use code insert so your code is formatted for easy reading.

Code Snippet.jpg

If you're receiving strings, hopefully with a LF, you can use a ring buffer/queue to save what you received. Then you can parse the message outside of the interrupt. Right now you're doing way to much processing inside the interrupt so you have a high chance of missing the next few bytes.

See this project https://github.com/karlyamashita/ParseRawData/wiki

 

Or you can use the Idle interrupt using the DMA

https://github.com/karlyamashita/Nucleo-G431RB_Three_UART/wiki

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

How are you going to determine the length/end of the input? Construct a line buffer holding that until the end, then process.

Avoid doing all this time wasting stuff in the interrupt or callback. If it take more than a byte-time you run the risk of losing data or overrunning.

The STM32F4 is going to interrupt for each byte

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..