cancel
Showing results for 
Search instead for 
Did you mean: 

Where do you get the Samtec ASP-203799-02 connector for the STLINK-V3SET?

J.Christ
Associate II

The STLINK-V3SET Suggest the following connector for one of the three cables included with it: Samtec ASP-203799-02. However, I cannot find this connector on Samtec or any corner of the internet other than the STLINK User manual. Where do you get this connector?

I see others have asked this question without a response. I can't post a l*nk to this topic as I'm a "new" member so here is a hint to the message:

" d " = .

" S " = /

community d st d com S s S question S 0D53W00000BKtMoSAL S stdc14-to-arm10-ribbon-cable-part-number

Jacob

1 ACCEPTED SOLUTION

Accepted Solutions
Andreas Bolsch
Lead II

Don't bother with these part numbers. Plain IDC 1.27mm male/female headers will do.

View solution in original post

3 REPLIES 3
AScha.3
Chief III

maybe STM found a way of some "copy protection" - by using a connector, only STM can give you...

i dont know.

i made my connector with a stLink V3 mods and some wires and resistors.

i never buy a cable for 26 € to connect a debug probe...

better to take another company, if they stay on this "model" .

If you feel a post has answered your question, please click "Accept as Solution".
J.Christ
Associate II

:\ Maybe, I found the mating connector by looking at the BOM for an STM dev board.

Samtec Inc.FTSH-107-01-L-DV-K

Samtec Inc.FTSH-105-01-L-DV-K

Andreas Bolsch
Lead II

Don't bother with these part numbers. Plain IDC 1.27mm male/female headers will do.