cancel
Showing results for 
Search instead for 
Did you mean: 

Virtual com port driver not properly installed

KPate.61
Associate II

ST Link V3 SET is giving error due to virtual com port not installed in computer

1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hi @KPate.6​ ,

A similar question is already asked here.

In the description of the STSW-STM32102 you can find:

Virtual COM Port driver installation package for Windows® operating systems: 98SE, 2000, XP, Vista®, 7, and 8.x.

Windows 10 does not require the installation of the Virtual COM Port driver anymore, as it is already built in.

So, if you use a Windows® operating systems: 98SE, 2000, XP, Vista®, 7, and 8.x try to uninstall the driver and reinstall the last version.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
KDJEM.1
ST Employee

Hi @KPate.6​ ,

A similar question is already asked here.

In the description of the STSW-STM32102 you can find:

Virtual COM Port driver installation package for Windows® operating systems: 98SE, 2000, XP, Vista®, 7, and 8.x.

Windows 10 does not require the installation of the Virtual COM Port driver anymore, as it is already built in.

So, if you use a Windows® operating systems: 98SE, 2000, XP, Vista®, 7, and 8.x try to uninstall the driver and reinstall the last version.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.