2026-01-29 4:41 AM - last edited on 2026-02-27 5:38 AM by KDJEM.1
Hi,
Can i use the NUCLEO-N657X0-Q board as custom ASIC over an Octal SPI style bus?
Thanks
Atchaiah
Solved! Go to Solution.
2026-01-29 6:05 AM - edited 2026-01-29 6:26 AM
@Atch123 wrote:
Can i use the NUCLEO-N657X0-Q board as custom ASIC over an Octal SPI style bus?
So if I assume I understood your question: that "Nucleo board" will play as a kind of slave of another OSPI master, the answer: that's not possible. OSPI embedded in all STM32 MCUs is always a master and cannot be configured as a slave.
2026-01-29 5:03 AM - edited 2026-01-29 5:56 AM
Hello @Atch123 and welcome to the ST community,
I don't know if you are colleagues (with this OP post). But that question was almost already asked there ..
2026-01-29 5:04 AM - edited 2026-01-29 5:04 AM
Welcome to the forum.
Please see How to write your question to maximize your chances to find a solution for best results.
Your question is unclear: what do you mean by "use the board as a custom ASIC"?
The STM32 is a microcontroller.
Does this thread help: STM32N6570-D: Is XSPI/OSPI for memory only, or also external peripherals ?
2026-01-29 6:05 AM - edited 2026-01-29 6:26 AM
@Atch123 wrote:
Can i use the NUCLEO-N657X0-Q board as custom ASIC over an Octal SPI style bus?
So if I assume I understood your question: that "Nucleo board" will play as a kind of slave of another OSPI master, the answer: that's not possible. OSPI embedded in all STM32 MCUs is always a master and cannot be configured as a slave.
2026-02-10 7:35 AM
Hello @Atch123 ,
Could you please state on this thread please? if your question has been answered please accept the post that has answered your question as solution, otherwise, we (as administrators) we will accept one of the posts listed above as a solution .
Thank you for your understanding.