cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL 56G3MAI not working with N657X0

alucart
Associate

Hi guys,
I'm try to use Camera FPC 22 pin cable with UVC mode. But it turn out screen are all black and error in console terminal is below

========================================
x-cube-n6-camera-capture v2.0.0 (3308d6b)
Build date & time: Jan 22 2026 09:34:57
   Compiler: GCC 12.3.1
HAL: 1.3.0
========================================
Start streaming YUV2 | 224x224@30fps
assertion "ret == CMW_ERROR_NONE" failed: file "Src/app_cam.c", line 173, function: CAM_Init
 
 
I used binary from "x-cube-n6-camera-capture-main"
I also try to re-compile with github project "STM32N6-GettingStarted-ImageClassification Application"
with header with cmw_camera.c USE_VD56G_SENSOR , still not success,
(debug then found that driver StartStreaming can ctx->write8 but not response at function about PollReg8(..);

Anyone have get experince how to make it work?ST_UVCL.png
1 REPLY 1
alucart
Associate

Updated : My camera still work (not broken) after re-compile with preprocessor # USE_VD56G3_SENSOR at 
github sample project : x-cube-n6-camera-capture-nucleo , need to //comment out some line
//cam_conf.mirror_flip = CAM_getFlipMode(sensor); at app_cam.c 

Then camera can display into my Window camera or VLC player.

But still no clue about why it not work at image classification project at by pass LCD pipeline..