cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U031K8U6 Download fail.

박인구
Associate II

hi~! 

I made a IOT prototype with STM32U031K8T6, but I can't download firmware.

The connection isn't working ad it should, can anyone tell me the issues with the attacked circuit ??

I've tried both j-link and st-link download tools. 

_0-1750678666419.png

 

please reply from users who have used STM32U031.   

14 REPLIES 14
Andrew Neil
Super User

Welcome to the forum.

 


@박인구 wrote:

I can't download firmware.


Please give more details -  see: How to write your question to maximize your chances to find a solution 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
Super User

The schematic looks okay.

If you feel a post has answered your question, please click "Accept as Solution".

...except for the repeatedly inserted R7 (NRESET pull-up), which is not necessary for any STM32 because a pull-up is available internally.

However, R7 is only unnecessary and not the cause of unsuccessful downloads. As @Andrew Neil already mentioned, more information is required for this, e.g. photos of the ST-LINK used, in the case of the ST-LINK/V2 also of the back.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Hl_st
ST Employee

Hello,

did you have set BOOT0 pin to HIGH before you were trying to download the firmware to MCU?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

박인구
Associate II

Thank you for your answer. As you can see in the circuit diagram, boot0 is fixed to low.

Thank you for your answer. I will attach the image of the ST-Link soon.

You accepted my statement as a solution.

How did you get it working?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
csocom
Associate II

Edit by ST Moderator: This post has been translated from Korean to comply with the ST Community Terms and Conditions (§10.2).

 

Seoul, 25 September 2025 The STM32U031K8U6 will not connect to the ST-Link SWD. Downloading is not possible.

I do not know the reason.

Have you managed to resolve this?

Debugging pins: 3.3V, SWDIO, SWCLK, NRESET, GND

NRSET is not used.

 

@csocom

The same request applies to your question: more information is required for this, e.g. photos of the ST-LINK used, in the case of the ST-LINK/V2 also of the back.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.