User Activity

STM8S001j3   SWIM PIN Not work, After hex file download (IAR EWSTM8 Compiler)8 pin port (SWIM) How to do in the firmware IAR.-DATASHEET 12page-Recommendation for SWIM pin (pin #8) sharingAs the NRST pin is not available on this device, if the SWIM...
I want STM32F103 to I2C mode testI can control <I2C Master Transmitter & Slave Receiver > mode But, I need -. When I2C Slave Mode: Slave Transmitter & Master Receiver example Code.example)Slave transmitterSlave receiverMaster transmitterMaster receiv...
Posted on July 13, 2018 at 10:29STM32F10x DAC (stm32f_ref Manual_RM0008, page248)........data for DAC channel2 to be loaded into DAC_DHR12LD [27:16] bits.What is correct DAC_DHR12LD[27:16] or DAC_DHR12RD[27:16]?? error wordI think  Right about  DAC_...
Kudos from