2023-03-05 8:35 AM
I am working on a schole projekt and there I neded to design a PCB that can talk to the PC over USB. whiel doing that I am not able to figure aout whie the USB connection dous not work if it is not set for programming.
In detail:
The USB Connection is ISOLATED with a ADUM3160.
When I set BOOT0 to HIGH for programming over USB, everything works fine.
When I set it to LOW for using it as a Virtual Com Port it dous not work, I triued other Middle ware states suche as HID but the same error code 43.
I trued enabeling the Pullup from the Isolater only five secondes after everything was initilysed but that did not work.
2023-03-07 2:10 AM
Hello @TFalk.1 and welcome to the Community :)
Have a look to this FAQ: USB device not recognized, it may help you.
Check the jumpers removed, and I advise you to validate your USB CDC configuration with a basic USB CDC device application in the STM32 USB training.
Best Regards,
Imen