- You can connect ST_UartRx to MIPI14_pin13, and ST_UartTx to Mipi14_pin14. This will allow the COM port that shows up when STLink created to use the Uart as Diagnostics. Careful: If the Uart also goes to a tranceiver IC or connector, then need to use wired-OR to combine the rx sources, a pullup (2K~10K) on the ST Rx pin, and a diode with cathode towards each Rx source (only 0's pass diodes).
- You can also connect USB_DP and USB_DM to a USB-C or other USB connector for diagnostics using VCP, refer to my other posts for a schematic. I like the USB-C connector as much more available when travelling.
Paul