2022-11-17 06:03 PM
Hi, can someone refer to the above MCU reference. This is my first time using the STM32 MCU chip on my embedded system. My question regarding the power up/down phases concerning specifically on STM32L433CCT6 IC ... Is it a must and critical to use some kind of power sequencing/power management IC to perform the function ? My board consists just serial and CAN ports, relays, digital input circuits and few external memory ICs. - Any specific power management IC suitable for the job? - Thank you in advance
Solved! Go to Solution.
2022-11-18 12:19 AM
Except for the STM32MPx family, no other member needs power sequencing or a power management IC, so it can be connected directly to a supply voltage. In the simplest case, even a battery is sufficient for this, as long as its voltage does not exceed the maximum value of 3.6V.
Does it answer your question?
Regards
/Peter
2022-11-18 12:19 AM
Except for the STM32MPx family, no other member needs power sequencing or a power management IC, so it can be connected directly to a supply voltage. In the simplest case, even a battery is sufficient for this, as long as its voltage does not exceed the maximum value of 3.6V.
Does it answer your question?
Regards
/Peter
2022-11-18 07:01 PM
Read the AN4555 and also look at the schematics of ST boards.
2022-11-20 06:04 AM
Yes Peter, thank you for the clarification
2022-11-20 06:06 AM
Many thanks. I hope you are not really scary as your nickname. Thank you again.