2015-03-17 2:42 PM
Greeting,
I'm facing an issue while trying to program STM32L151C6 using STM32F4 Discovery board as programmer. What I did are the following:1. I removed CN3 jumpers from STM32F4 Discovery board page 14 in [][1]2. I connect NRST, SWDIO, GND, SWCLK, Vdd to my target STM32L151C6 SWD pins except SWO ( I kept it floating)Pin:number CN2 (STM32L151C6) Pin:1 Vdd Pin:2 SWCLK (PA14) Pin:3 GND Pin:4 SWDIO (PA13) Pin:5 NRST (NRST) Pin:6 SWO (No Contact)
3. I used STM32 ST-Link Utility V2.2.6 to test SWD.The result is ''Cannot connect to ST-Link''I've attached the schematic for my circuit design.I really appreciate your prompt help guys to facilitate this issue.2016-01-31 7:52 PM
Problem solved!
The orientation of the MCU was incorrect. I missed understand that the Pin1 is at the top left according to STM32L476xx Datasheet page 59/232. Actually, Pin1 is at bottom left according to the datasheet page 223/232. I could not find the 'New'. I have used Ctrl+f to search for it. There is no such thing. Thank you for your help.