cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H755 emmc compatibility - IS22TF08G-JCLA2

sarun
Associate III

Hello,

In the RM0399 58.1 it is mentioned that EMMC is supported up to Version 4.51. I want to use the part  IS22TF08G-JCLA2 which supports a number of emmc interfaces up to 5.1 are these parts compatible? 

1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hello @sarun ,

The HS200 mode supported in IS22TF08G is compatible with STM32H755.

KDJEM1_1-1718103452213.png

 

KDJEM1_0-1718103370314.png

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
KDJEM.1
ST Employee

Hello @sarun ,

The HS200 mode supported in IS22TF08G is compatible with STM32H755.

KDJEM1_1-1718103452213.png

 

KDJEM1_0-1718103370314.png

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

sarun
Associate III

Thank you @KDJEM.1  for confirmation