2024-06-05 11:50 PM - edited 2024-06-07 12:21 AM
Hello,
In the RM0399 58.1 it is mentioned that EMMC is supported up to Version 4.51. I want to use the part IS22TF08G-JCLA2 which supports a number of emmc interfaces up to 5.1 are these parts compatible?
Solved! Go to Solution.
2024-06-11 03:58 AM
Hello @sarun ,
The HS200 mode supported in IS22TF08G is compatible with STM32H755.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-11 03:58 AM
Hello @sarun ,
The HS200 mode supported in IS22TF08G is compatible with STM32H755.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-11 04:00 AM
Thank you @KDJEM.1 for confirmation