2024-05-14 03:42 PM - last edited on 2024-05-14 06:48 PM by SofLit
hi guys,
I hope this message finds you well.
I am currently working with the STM32H743Eval2 evaluation board, and I'm facing a challenge with the smaller pins on the board. Specifically, I've noticed that the standard-sized pins do not fit in these smaller pin slots. how can I reach these pins.
Thank you very much for your time and assistance.
Solved! Go to Solution.
2024-05-15 03:27 AM - edited 2024-05-15 03:28 AM
Hello,
Internally we have a such adapters to access that connectors on H7/F7 Eval boards:
But unfortunately they are not available on the market
I would suggest:
1- The usage of that kind of "clips" (I don't know if this is the right naming) that you can attach directly to the pin:
2- Solder wires on the connector pins base if you're familiar with soldering.
2024-05-14 05:15 PM
Perhaps pull the BoM from the "CAD Resources" tab on the product page. Determine the header type and pitch from the BoM
2024-05-14 05:24 PM
https://www.st.com/en/evaluation-tools/stm32h743i-eval.html
https://www.st.com/en/evaluation-tools/stm32h743i-eval.html#cad-resources
https://www.st.com/resource/en/bill_of_materials/mb1246_bom.zip
CN11 / CN12 Header,2*20,1.27*2.54mm,with positioning pin,SMT,333240M121
2024-05-15 03:27 AM - edited 2024-05-15 03:28 AM
Hello,
Internally we have a such adapters to access that connectors on H7/F7 Eval boards:
But unfortunately they are not available on the market
I would suggest:
1- The usage of that kind of "clips" (I don't know if this is the right naming) that you can attach directly to the pin:
2- Solder wires on the connector pins base if you're familiar with soldering.