2024-07-23 11:16 PM - last edited on 2024-07-24 01:55 AM by SofLit
2024-07-24 12:41 AM
Hello @durgamaravind1077 and welcome to the ST Community
There is no Boards (Nucleo, DK or Eval) that use the STM32H735IGT6. The only board that embeds an STM32H735 is the STM32H735G-DK (Based on the STM32H735IGK6 MCU).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-24 12:45 AM
which nucleo board is suitable.
2024-07-24 01:04 AM
As I've already said, "There is not a Nucleo board based on this MCU". The Nucleo boards are evaluation boards that are available only for a few MCUs and not all of them.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-24 02:43 AM
@durgamaravind1077 wrote:Which NUCLEO board is suitable for STM32H735IGT6 microcontroller.
As always, go to the Product Page for that chip, on the 'Tools & Software' tab look for 'Evaluation Tools':
https://www.st.com/en/microcontrollers-microprocessors/stm32h735ig.html#tools-software
Follow the link:
As @STTwo-32 said, the only option is the STM32H735G-DK:
https://www.st.com/en/evaluation-tools/stm32h735g-dk.html
2024-07-24 02:54 AM
Can You recommend any NUCLEO board for stm32h7 series ?
2024-07-24 03:03 AM
Again, go to the STM32H7 page, and look on the 'Tools & Software' tab:
https://www.st.com/en/microcontrollers-microprocessors/stm32h7-series.html#tools-software
That 'Product evaluation tools' link takes you to:
2024-07-24 03:04 AM - edited 2024-07-24 03:19 AM
Nucleo-H723 is the closest to the H735.
Except for some missing peripherals, these MCUs are 100% compatible.
But don't forget: the Nucleo-board has almost no extra stuff equipped: no external RAM, no flash, no... other stuff.